This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6000的bootloader问题

    TI的bootloader文档里讲过bootloader要用汇编语言来写,因为还没有建立c语言运行环境。但是,我看到网上有人用c语言弄的bootloader,于是我也试了试,但是一直有问题。

    我用的DSP型号是c672x,采用的方法是写两个c文件,一个boot.c,一个appmain.c(自己的应用代码)。boot.c里装着void boot()函数。boot.c的代码放到Flash前1KB,appmain.c代码放到1KB以后位置。具体方法是这位朋友弄的http://wenku.baidu.com/view/5dd6cc62caaedd3383c4d354.html

  c672x只有13跟地址线(包括em_ba1),所以Flash高位地址线需要扩展GPIO,这样读取Flash的时候,要手动换页。下面是我的boot.c的代码,顺序是:配置锁相环——配置emif——配置GPIO为高位地址线——for循环搬运代码——使用c_int00()函数寻找main函数入口。

   最开始的时候,配置锁相的那部分代码是作为一个函数调用的,但是总出现问题,后来我直接把配置锁相代码拿到boot函数里了,去掉函数调用这一步。正常了。难道是因为bootloader里面没有设置堆栈?

    boot.c中间有一段代码,是while输出方波死循环(已被注释掉),如果不注释的话,dsp上电执行到这一步,正常配置锁相、emif、gpio,然后输出所要的方波,但如果注释掉while死循环,就发现,虽然前面的都执行正确,但是搬运代码的for循环不正常,找不出规律,有时貌似一直在搬运,但是却不见gpio有所改变,所以又像没在搬运,但emif却一直在输出读信号。

    成功过一次,上电,很快完成搬运,然后dsp对着sdram一顿疯狂操作(不是我主程序要求的),过了得五分钟才看到我主程序里要求的现象。

    另外,这个dsp是好使的,因为我按照TI给的“Using the TMS320C672x Bootloader”这个文档的方法,是可以正常boot的。只是得使用AIS格式的数据流。

    下面是我的boot.c代码:

//#include <stdio.h>
#define IRAM_ADDR      0x10000400                    //内部RAM地址,从这里开始放用户应用代码
#define FLASH_ADDR  0x90000400                   //Flash地址,404位置存放代码长度,从408开始存放用户代码
/****************************************************/
/*GPIO设置*/
#define PFUNC1       0x45000010
#define PDIR1       0x45000014
#define PDOUT1      0x45000018
/****************************************************/
#define EMIF_A1CR           0xF0000010
/****************************************************/
#pragma CODE_SECTION(boot,".bootload");
extern far void c_int00();
void boot()
{
 unsigned int i;
 unsigned int addr1;
 unsigned char a13,a14,a15,a16,a17;
 unsigned short int code_length;
/****************************************************/
//开始配置锁相(原来这部分代码是一个独立函数,在这个地方调用配置锁相函数)

#define TIBOOT_PLL_REG_BASE_ADDR        (0x41000000u)
#define TIBOOT_PLL_PLLCSR               (TIBOOT_PLL_REG_BASE_ADDR + 0x100u)
#define TIBOOT_PLL_PLLM                 (TIBOOT_PLL_REG_BASE_ADDR + 0x110u)
#define TIBOOT_PLL_PLLDIV0              (TIBOOT_PLL_REG_BASE_ADDR + 0x114u)
#define TIBOOT_PLL_PLLDIV1              (TIBOOT_PLL_REG_BASE_ADDR + 0x118u)
#define TIBOOT_PLL_PLLDIV2              (TIBOOT_PLL_REG_BASE_ADDR + 0x11Cu)
#define TIBOOT_PLL_PLLDIV3              (TIBOOT_PLL_REG_BASE_ADDR + 0x120u)
#define TIBOOT_PLL_PLLCMD               (TIBOOT_PLL_REG_BASE_ADDR + 0x138u)
#define TIBOOT_PLL_PLLSTAT              (TIBOOT_PLL_REG_BASE_ADDR + 0x13Cu)
#define TIBOOT_PLL_PLLALNCTL            (TIBOOT_PLL_REG_BASE_ADDR + 0x140u)
#define TIBOOT_PLLENABLE                (0x01u)
#define TIBOOT_PLLDISABLE               (0x00u)
#define TIBOOT_PLLPWRDN                 (0x02u)
#define TIBOOT_PLLPWRUP                 (0x00u)
#define TIBOOT_PLLOSCPWRDN              (0x04u)
#define TIBOOT_PLLOSCPWRUP              (0x00u)
#define TIBOOT_PLLRESET                 (0x08u)
#define TIBOOT_PLLRESETRELEASE          (0x00u)
#define TIBOOT_PLLSTABLE                (0x40u)
#define TIBOOT_PLLUNSTABLE              (0x00u)
#define TIBOOT_PLLLOCKED                (0x20u)
#define TIBOOT_PLLNOTLOCKED             (0x00u)

/* FOR PLLCMD */
#define TIBOOT_PLLGOCLR                 (0x0000u)
#define TIBOOT_PLLGOSET                 (0x0001u)

 

/* FOR PLLSTAT */
#define TIBOOT_PLLGODONE                (0x0000u)
#define TIBOOT_PLLGOWAIT                (0x0001u)

/* FOR ALNCTL */
#define TIBOOT_PLLALN1                  (0x0001u)
#define TIBOOT_PLLALN2                  (0x0002u)
#define TIBOOT_PLLALN3                  (0x0004u)

/* FOR PLLDIV0,1,2,3 and OSCDIV1 */
#define TIBOOT_DIVENABLED               (0x8000u) 

            
   *(volatile unsigned int *)TIBOOT_PLL_PLLDIV0 = TIBOOT_DIVENABLED | 0x00000000;
   *(volatile unsigned int *)TIBOOT_PLL_PLLM = 0x00000014;


   *(volatile unsigned int *)TIBOOT_PLL_PLLDIV1 = TIBOOT_DIVENABLED | 0x00000001;
   asm("  nop 4");
   asm("  nop 4");

   *(volatile unsigned int *)TIBOOT_PLL_PLLDIV2 = TIBOOT_DIVENABLED | 0x00000003;
   asm("  nop 4");
   asm("  nop 4");

   *(volatile unsigned int *)TIBOOT_PLL_PLLDIV3 = TIBOOT_DIVENABLED | 0x00000003;


   *(volatile unsigned int *)TIBOOT_PLL_PLLALNCTL = TIBOOT_PLLALN1 | TIBOOT_PLLALN2 | TIBOOT_PLLALN3;
   *(volatile unsigned int *)TIBOOT_PLL_PLLCMD = TIBOOT_PLLGOSET;

   while (*(volatile unsigned int *)TIBOOT_PLL_PLLSTAT == TIBOOT_PLLGOWAIT){
      *(volatile unsigned int *)TIBOOT_PLL_PLLCMD = TIBOOT_PLLGOCLR;
   }

     for(i=0; i< 7;++i) {};

   *(volatile unsigned int *)TIBOOT_PLL_PLLCSR = TIBOOT_PLLENABLE | TIBOOT_PLLRESETRELEASE;
    for(i=0; i < 3850; ++i) {};

//配置锁相结束
/****************************************************/

配置emif
   *(int *)EMIF_A1CR =   ( 1 << 31) //WE Strobe mode
        | ( 0 << 30) // EW       : Disable extended wait mode     
        | ( 0 << 26) // W_SETUP  :  10 ns @ 100 MHz            
        | ( 9 << 20) // W_STROBE           
        | ( 3 << 17) // W_HOLD             
        | ( 0 << 13) // R_SETUP            
        | ( 9 <<  7) // R_STROBE            
        | ( 3 <<  4) // R_HOLD            
        | ( 0 <<  2) // TA              
        | ( 1 <<  0); // ASIZE    :  16-bit data bus               
/****************************************************/
 /*Flash高位地址线配置*/
 *(int *)PFUNC1=(0xF<<28)//保留位必须写入0
    |(0xE<<24)
    |(0<<20)
    |(0<<16)
    |(0<<12)
    |(0<<8)
    |(3<<4)
    |(0xF<<0);
 *(int *)PDIR1=(0xF<<28)//保留位必须写入0
    |(0xE<<24)
    |(0<<20)
    |(0<<16)
    |(0<<12)
    |(0<<8)
    |(3<<4)
    |(0xF<<0);
 *(int *)PDOUT1=(0<<31)//AFSR_A17
    |(1<<30)
    |(0<<29)//ACLKR_A15
    |(0<<28)//AFSX_A16
    |(0<<27)//AHCLKX_A13
    |(0<<26)//ACLKX_A14
    |(1<<25)//AMUTE
    |(0<<16)//Reserved_0
    |(0<<6)//AXR15~AXR6
    |(1<<5)//AXR5
    |(0<<4)//AXR4
    |(1<<3)//AXR3
    |(0<<2)//AXR2
    |(1<<1)//AXR1
    |(0<<0);//AXR0
      //while(1)                                                                                     
      //{                                                                                       
      // *(int *)PDOUT1=*(int *)PDOUT1 | 0x01;                                                    
      // for(i=0;i<100;i++)                                                                        
      // {}                                                                                        
      // *(int *)PDOUT1=*(int *)PDOUT1 & 0xfffffffe;                                               
      // for(i=0;i<100;i++)//输出一个方波                                                        
      // {}                                                                                                                                                                                  
   //} 

//搬运代码的for循环
 code_length=*(unsigned short *)(FLASH_ADDR+4);//这个位置存放着要搬运的代码长度


 for(i=0;i<code_length;i++)
 {
   addr1=FLASH_ADDR+8+2*i;
   addr1=addr1>>1;
   a13=(addr1>>13) & 0x01;//地址线A13
   a14=(addr1>>14) & 0x01;
   a15=(addr1>>15) & 0x01;
   a16=(addr1>>16) & 0x01;
   a17=(addr1>>17) & 0x01;
  *(int *)PDOUT1=(a17<<31)//AFSR_A17
     |(1<<30)
     |(a15<<29)//ACLKR_A15
     |(a16<<28)//AFSX_A16
     |(a13<<27)//AHCLKX_A13
     |(a14<<26)//ACLKX_A14
     |(1<<25)//AMUTE
     |(0<<16)//Reserved_0
     |(0<<6)//AXR15~AXR6
     |(1<<5)//AXR5
     |(0<<4)//AXR4
     |(1<<3)//AXR3
     |(0<<2)//AXR2
     |(1<<1)//AXR1
     |(0<<0);//AXR0 
  *(unsigned short *)(IRAM_ADDR+2*i)=*(unsigned short *)(FLASH_ADDR+8+2*i);
 }

 c_int00();    
}