各位TI工程师好!
请问下C6657的GPIO16~GPIO31应该如何来配置为输出或输入?我看将GPIO的PDF文档上只能对GPIO0~GPIO15进行输入输出控制。比如DIR寄存器就只有低16bit有效,只能对GPIO0~GPIO15进行配置。
另外我想使用GPIO22作为外部中断信号引脚,那除了我在中断配置映射上进行二次映射,还需要做什么配置,才能接收到中断啊,目前我的板卡上接收不到中断!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位TI工程师好!
请问下C6657的GPIO16~GPIO31应该如何来配置为输出或输入?我看将GPIO的PDF文档上只能对GPIO0~GPIO15进行输入输出控制。比如DIR寄存器就只有低16bit有效,只能对GPIO0~GPIO15进行配置。
另外我想使用GPIO22作为外部中断信号引脚,那除了我在中断配置映射上进行二次映射,还需要做什么配置,才能接收到中断啊,目前我的板卡上接收不到中断!
1. GPIO31~16这些引脚的设置跟GPIO15~0是同一个寄存器,GPIO用户手册有点老了,没有更新信息,设置对应的31~16位就可以了
2. 可以参考置顶贴里STK_C6657的GPIO中断例程。
http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx?pi239031348=2