我们自己做的板子是AM3352通过MCASP0连接PCM3168A,DIN和DOUT分别使用AR0和AR2。现在PCM3168A需要配置6路输出和1路输入,通过TDM将6个MIC的数据传输到AM3352上。3352使用的晶振是24M,MCASP为主模式。PCM3168的6路MIC配置为32K 24bit。请教一下这样的配置3352的MCASP能正常传输吗?stareware里面没有主模式和TDM的示例,有点无从下手。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.