This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914A 高位 D11,D10无输出



我设计了一款914A的板子,在mode设置上(如下图):

 1,如果电阻为3K,则会提示初始化senser失败。

2,将电阻改成8K(此处电压在0.79V左右),初始化成功,画面有图像,显示绿屏,用示波器测试,D11,D10没有输出。

3,我用客户提供的板子,在同样的环境下(软件相同,前端是913,客户板子是用10K/3K),客户的板子工作正常,D11和的D10有数据波形,画面正常(不会出现绿屏)。

4,目前两份原理图是一样的,软件配置也相同。

5,我准备调试了几天都没有结果,现在继续支持,可以电话我:17089493266 或是0756-3980999 分机8851