This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询DM642设计问题



我选用的DSP是DM642, 1、DM642只用于做加密算法,视频管脚不用,是否可以直接悬空处理;2、SDRAM芯片配置EMIFA总线CE0,NORFLASH配置在CE1空间,FPGA 异步SRAM分配在CE2空间,SRAM分配在CE3空间,串接33欧姆电阻后,是否还需要外部总线驱动芯片增加驱动力?只用了32位数据宽度,高32位数据位不用,是否可以直接悬空处理?3、DM642的PCI管脚与PC104PLUS电平标准兼容吗?

  • 1. 对于不用管脚的处理规则是:除特别说明外,输入管脚用上拉,或下拉电阻设置为固定电平,输出管脚可以悬空处理。

    2. 就是说EMIF上接了4个外设,根据DM642的手册5.8.1节的说明,需要用IBIS模型进行信号完整性分析。

    3. 高位不用的信号可以悬空处理。

    4. DM642的PCI是符合PCI 2.2规范的。