你好,我使用DM8127自己做的板子,使用SD卡启动,上电后,串口终端打印如下信息后,就卡死了,已经排除了不是DDR3的问题,我现在手上有仿真器,请问如何使用仿真器调试内核,观察内核卡在哪个函数呢,有没有相关技术文章介绍呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我使用DM8127自己做的板子,使用SD卡启动,上电后,串口终端打印如下信息后,就卡死了,已经排除了不是DDR3的问题,我现在手上有仿真器,请问如何使用仿真器调试内核,观察内核卡在哪个函数呢,有没有相关技术文章介绍呢?谢谢!
你好,我是在uboot的stage1第一阶段进行DDR配置的,在内核中不知道有没有进行DDR配置,我对内核源码不是很熟悉
可以用仿真器连上ARM
不要加任何GEL脚本
看看PC指针停在什么位置,然后到.map文件里找对应函数
你好,能说的再详细一些吗?
当使用仿真器观察内核卡住的位置时,8148的启动模式应该选择成什么呢,我现在是SD卡启动(BTmode[4..0]=10111)是否可以。
非常感谢!