我使用的是TMS320C6657芯片,DDR3存储器需要设计8GB,目前市面上的DDR3最大容量只有1GB(8Gb),这样我需要外接8片DDR3存储器,请问从驱动能力上讲TMS320C6657能驱动得了8片DDR3存储器吗?这样设计有什么风险吗?我选用的DDR3存储器是8Gb(128 Meg x 8 x 8 banks)的DDR3存储器。
另外请问一下DDR3的走线,包括数据线、地址命令线和时钟线的最大走线长度有什么限制?
请回复,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的是TMS320C6657芯片,DDR3存储器需要设计8GB,目前市面上的DDR3最大容量只有1GB(8Gb),这样我需要外接8片DDR3存储器,请问从驱动能力上讲TMS320C6657能驱动得了8片DDR3存储器吗?这样设计有什么风险吗?我选用的DDR3存储器是8Gb(128 Meg x 8 x 8 banks)的DDR3存储器。
另外请问一下DDR3的走线,包括数据线、地址命令线和时钟线的最大走线长度有什么限制?
请回复,谢谢!
C6657 DDR3最大能支持到8GB。
走线请参考下面的DDR3布线文档。
http://www.ti.com/lit/an/sprabi1b/sprabi1b.pdf
谢谢您的回复。
您推荐的文档我看过了。我想问的是:目前市面上的DDR3最大容量只有1GB(8Gb),这样我需要外接8片DDR3存储器,请问TMS320C6657能驱动得了8片DDR3存储器吗?这样设计有什么风险吗?
文档里面没有答案啊。请一定回复一下。非常感谢!
看了一下数据手册不支持8片8bit DDR3的拓扑结构。
6.11.1 DDR3 Memory Controller Device-Specific Information
http://www.ti.com/lit/ds/symlink/tms320c6657.pdf
我从文档中看到可以支持如下拓扑结构:
The DDR3 electrical requirements are fully specified in the DDR Jedec Specification JESD79-3C.
Standard DDR3 SDRAMs are available in 8- and 16-bit versions, allowing for the following bank
topologies to be supported by the interface:
• 36-bit: Three 16-bit SDRAMs (including 4 bits of ECC)
• 36-bit: Five 8-bit SDRAMs (including 4 bits of ECC)
• 32-bit: Two 16-bit SDRAMs
• 32-bit: Four 8-bit SDRAMs
• 16-bit: One 16-bit SDRAM
• 16-bit: Two 8-bit SDRAM
但是我看到TMS320C6657的DDR控制器有两个时钟使能信号,两个时钟输出信号,两个片选信号,是不是可以控制两组DDR存储器,一组DDR存储器包含Four 8-bit SDRAMs,两组DDR存储器就包含八个8-bit SDRAMs。不知我理解的对不对?
请参考下面的帖子,C6657 最大只支持4GB DDR3.
http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/147424.aspx
您好,帖子我看了。我还有一些疑问,如下:
TMS320C6657的DDR接口有两个时钟信号(DDRCLKOUTP0/1,DDRCLKOUTN0/1),两个芯片使能信号(DDRCE0/1),两个时钟使能信号(DDRCKE0/1),两个OTD信号(DDRODT0/1)。这些信号为什么会有两组,我看参考设计实际只使用了一组,那么请问一下两组信号的意图是什么?谢谢!
请参考下面的框图。
Dual Rank DDR3 Implementation
http://www.ti.com/lit/an/sprabi1b/sprabi1b.pdf
TMS320C6657外部的DDR3设计为Dual Rank,最大容量是不是可以达到8GB?因为单Rank最大可以支持4GB,所以Dual Rank最大容量可以达到8GB。我的理解是否正确?很重要!请一定回复。谢谢!
请看下面e2e的回复。
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/654058/2407898#2407898
您好,帖子我看了,可还是不清楚使用Dual Rank,DDR3最大容量是否能做到8GB。
我理解TMS320C6657外部的DDR3单Rank最大可以支持4GB,所以Dual Rank最大容量可以达到8GB。请问对不对?如果不对,请说明一下原因,也加深我对这个片子的理解。
很重要。非常感谢!