Hello 您好,
目前想用C6657开发产品,产品对nand flash的容量要求比较高 >=8GB, 不知道硬件上如何连接?
根据memory map,CS1~CS4,最大只能支持 64MB*4 = 256MB的容量,是否硬件架构就不能在EMIF上接口上连接?
非常感谢!
BRS,
Meng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
256MB的容量只针对使用地址线的异步Memory,Nand flash是不用地址线的,所以最大容量没有限制。这在EMIF user guide上有说明。
Note—The 64MB limit per chip select applies only for asynchronous memories
that use the EMIF16 address bus for addressing - typically ASRAM and NOR
flash. NAND flash uses the data bus as a multiplexed data/address bus and does
not use EMIF16 address pins for addressing (Only CLE and ALE signals use
the address bus. Refer to Section 3.1 ‘‘NAND Flash Mode’’ for more details).
So NAND Flash > 64MB can be supported on one chip select.
http://www.ti.com/lit/ug/sprugz3a/sprugz3a.pdf
硬件连接参考上面的文档3.1.1 Connecting to NAND Flash。