This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于--relaxed_ansi编译成功,运行出问题



由于需要使用...代表不定参数,故放开了--relaxed_ansi这个选项,能编译通过,但是运行时,发现采集的数据都不对了,好像是没有对齐的问题,但不用该选项时一切正常,这怎么能解决呢?难道时编译选项--relaxed_ansi的问题。

'Building file: ../source/main.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv5/tools/compiler/c6000_7.4.4/bin/cl6x" -mv6740 --abi=coffabi -Ooff -g --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.4/include" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/drivers" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/include/c674x/c6748" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/include/hw" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/include" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/include" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/include/nandlib" --include_path="Z:/sl100/sl100_uav_onboard_ccs5p5/sl100_uav_onboard_ccs5p5/StarterWare/include/c674x" --include_path="/StarterWare/include/nandlib" --relaxed_ansi --define=c6748 --display_error_number --diag_suppress=383 --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="source/main.pp" --obj_directory="source"  "../source/main.c"


怎么办?谢谢