This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X poweroff 失败了?



SDK 2.00.01.07 linux4.1.13 

root@am335x-evm:~# poweroff

Broadcast message from root@am335x-evm (ttyS0) (Sat Jan  9 00:16:43 2016):
The system is going down for system halt NOW!
INIT: Switching to runlevel: 0
INIT: Sending pUIM SYSFS Node Not Found
Stopping telnet daemon.
Stopping system message bus: dbus.
Stopping syslogd/klogd: stopped syslogd (pid 644)
stopped klogd (pid 647)
done
Stopping thttpd.
stopping statd: done
ALSA: Storing mixer settings...
/usr/sbin/alsactl: save_state:1590: No soundcards found...
Stopping rpcbind daemon...
done.
Stopping Lighttpd Web Server: no /usr/sbin/lighttpd found; none killed
lighttpd.
Deconfiguring network interfaces... done.
Disabling thermal zones...
/etc/rc0.d/K98thermal-zone-init: line 13: /sys/class/thermal/thermal_zone*/mode: No such file or directory
Sending all processes the TERM signal...
Sending all processes the KILL signal...
Unmounting remote filesystems...
umount: can't forcibly umount mnt: Invalid argument
Deactivating swap...
Unmounting local filesystems...
[   44.808746] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
[   47.145633] musb-dsps 47401c00.usb: otg: usb_otg_unregister_hcd: device not registered to otg core
[   47.154878] musb-hdrc musb-hdrc.1.auto: remove, state 4
[   47.160220] usb usb2: USB disconnect, device number 1
[   47.166894] musb-hdrc musb-hdrc.1.auto: USB bus 2 deregistered
[   47.173145] musb-dsps 47401400.usb: otg: usb_otg_unregister_hcd: device not registered to otg core
[   47.182292] musb-hdrc musb-hdrc.0.auto: remove, state 4
[   47.187618] usb usb1: USB disconnect, device number 1
[   47.194032] musb-hdrc musb-hdrc.0.auto: USB bus 1 deregistered
[   47.203710] reboot: System halted

这是关机失败了吗?死机了?