我使用TMS320C6657芯片,NAND Flash容量需要做到16GB(128Gb),需要外接两个8GB的NAND Flash芯片,我想使用EMIF16接口的EMIFCE0/1和EMIFWAIT0/1信号实现对两个NAND Flash的访问(其余的信号两个NAND Flash共用),不知这样做有没有问题?请不吝指教。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用TMS320C6657芯片,NAND Flash容量需要做到16GB(128Gb),需要外接两个8GB的NAND Flash芯片,我想使用EMIF16接口的EMIFCE0/1和EMIFWAIT0/1信号实现对两个NAND Flash的访问(其余的信号两个NAND Flash共用),不知这样做有没有问题?请不吝指教。谢谢!
谢谢您的回复。对于两个NAND Flash的就绪(R/B#)信号,是不是分别接到TMS320C6657的EMIFWAIT0和EMIFWAIT01就可以了?
对于两个NAND Flash的就绪(R/B#)信号,是不是分别接到TMS320C6657的EMIFWAIT0和EMIFWAIT01就可以了?请回复。谢谢了!
是的,EMIF16手册上有参考框图。
3.1.1 Connecting to NAND Flash
http://www.ti.com.cn/cn/lit/ug/sprugz3a/sprugz3a.pdf