您好:
我在CCS5.2的编译环境下,编译5509A,在调用的dsplib3.00时,出现
"C:\c55_lp\c55_dsplib_3.00\lib\55xdspx_r3.lib<fir2.obj>" specifies "C55x CPU
Rev 3.x", which is not compatible with "C55x CPU Rev 2.x" specified in a
previous file or on the command line
这应该是DSP的架构较老,如何在该5509A,使用dsplib3.00.如果在silicon version选择5505或者5515编译能够通过。