This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

spectrum digital XDS560 V2 USB Debug 连接问题



我正在使用XDS560 V2 jtag工具调试i的tci6616芯片,之前USB连接一切正常,不过我升级了JTAG工具的固件之后,提示如下错误:

==============================================================================

[Start: Spectrum Digital XDS560V2 STM USB Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\wepan\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\xds560v2pro.xsvf
The library build date was 'Jul 27 2016'.
The library build time was '17:21:41'.
The library package version is '6.0.407.3'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Receive::dtc_io
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Receive::dtc_io

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-252' (0xffffff04).
The title is 'SC_ERR_ECOM_OPERATE'.

The explanation is:
An attempt to operate the USCIF interface via USCIF ECOM has failed.

[End: Spectrum Digital XDS560V2 STM USB Emulator_0]

=========================================================================

Firmware version 2.2.0.5

我已经按照说明上的文档设置

dtc_conf set _bootForce=true
dtc_conf set  _fpgaForceLoad=false
但是现在每次发送命令都是上述结果,请问该怎么解决,谢谢!
补充一下:USB status 测试时,usb test loopback 10次 passed