This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168通过PCIe与ML605连接时出现问题



Dear all,

   我在使用EVM8168并通过PCIe接口与xilinx的ML605开发板连接时出现了问题,EVM8168无法检测到ML605。

   ML605的PCIe配置为x1 gen1,在台式机上验证通过,并且能用PciTree软件对BAR空间进行读写。

    当插入到EVM8168上时,查看PCI设备,发现无法找到ML605。

   我的软件环境为DVRRDK_01.09.00.16,kernal 2.6.37已经按照RC guide中调到的对SW5进行设置,并通过代码产生RST信号。

   请专家帮忙分析下,谢谢!