This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2G 开机问题



应用EVM K2G开发板的时候;

直流线性稳压电源供电,12V(MAX 5A);

在开始的时候偶尔出现启动不了,现象如下:

输入电压:12V  

输入电流:0.06~0.08A

VCC3.3V_BMC(TP195):  3.3V

VCC12V0_DC_IN(TP63):  4.06V

LED: LD9,LD12,亮

          LD14 (VINPUT above 13V or below 11V&Current above 5A)亮;

          其他LED都不亮;

BMC LCD  背光亮,无内容显示。

在SW3(0000)Sleep/No Boot 和 SW3(0111)MMC/SD Boot  都出现过这种现象,初步推测是BMC没有加载;

开始的时候,偶尔出现这个问题;出现上几次电 ,就可以正常加载。

如今每次都出现,只有间隔很长时间(大于4小时)开一次机,才可能正常加载,请问该问题我们应该如何解决?