This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello 您好,
目前想用C6672开发一个新项目,但是体积受限,C6672 DSP 必须外接 8GB DDR3, 我们到网上查了,DDR3 1.5V 最大尺寸也就1GB,这样我的接8个DDR3
才可以,这样板子的体积占用太大,不知道是否有 2GB 大小尺寸的DDR3,适合C6672 外接,这样,我们接4个2GB的就可以达到8GB,非常感谢!
另外,一般用DDR3 都要多一块用来做ECC用,如果不用ECC,可以吗?如果可以,会有负面影响?
谢先!
BRS,
Meng
1. 这个需要咨询memory vendor.
2. 可以不用贴ECC,很多EVM就没贴ECC。