This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
文档第77页对未使用的SPI引脚的要求有一个注释,如下:
Note—*: The above recommendations are based on the peripheral being
unused and no traces attached. If traces are attached to any of the peripheral
input pins, added pull-up (to DVDD18) or pull-down (to VSS) resistors
(4.7 k) are needed.
这段文字怎么解释?尤其是“traces are attached to any of the peripheral input pins” 是什么意思?
谢谢!