This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6614 EMIFA使用nor+nand flash的问题



如题,请教以下问题:

1)我想使用64MB的nor flash,16b数据接口,地址最高为A24怎么连接?需要占用几个片选?

2)在以上基础上,我想再接一片nand flash,可以用哪个片选?最大可以访问多大容量的nand flash?

3)最后还需要占用一个片选用来访问另一个小的外部存储器(512B)

  • 1. A24需要用外部管脚如GPIO管脚控制,EMIF16每个片选最大只能支持2^24x16bit=32MB.

    2. 跟nor flash不要用同一个片选信号就可以了。因为nand flash不是地址寻址,所以没有大小限制。

    3. 看这是什么类型的存储器,EMIF16是否支持。