This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 支持IMX290 WDR输出multi frames (frame by frame, or line by line) in a linear mode 吗?



A WDR sensor shorts every frame with multiple exposure times (in general between 2 ~ 4, with
an exposure time ratio between 4x ~ 16x). The WDR sensor then outputs
1) Either multi frames (frame by frame, or line by line) in a linear mode
2) Or a single frame with higher bit depth (16 bits for example)
3) Or a single frame in a companded (compressed) mode.

这是8127RDK的WDR 相关文档说明,文档仅介绍了8127可以接收上述第3)种数据格式。请问8127支持接收上述第1)种 wdr 数据格式吗?