各位前辈好,本人是名新手,刚接触这一领域,有些问题想请教各位,望不吝赐教!
现在我有一个C6655的板子,想把基于opencv的算法(跟踪方面的,如KCF)移植上去,有没有什么可行的方案,
前期已经查阅了一些资料,
1、processors.wiki.ti.com/.../C66x_opencv,这个链接里讲的opencv移植需要用到第三方产品,看的我一头雾水
2、software-dl.ti.com/.../index_FDS.html,这个是VLIB,一个用于视频分析的库,里面的介绍是:VLIB is a software library of more than 100 royalty-free kernels from Texas Instruments that accelerates video analytics development and increases performance up to 10 times. 看了里面的函数,总体感觉功能还是有点少,而且和opencv没有太大的联系
3、software-dl.ti.com/.../index_FDS.html,这个是OpenCV 1_0_0_0,是TI对opencv 2.4.9改写后的库,可以支持TI K2H、Sitara devices等,里面的介绍是:This is a GA release of the OpenCV (www.opencv.org) for TI K2H & compatible Sitara devices.This release is based on the OpenCV version 2.4.9.
The deliverables in this release include tar archive for the K2H & compatible Sitara devices. The release contains opencv source package, pre-built libraries (both static & shared), examples & documentation
对K2H,我不太了解,Sitara devices基本上都是ARM类型的板子,www.ti.com/.../overview.html,这个是总览表。可我要找的是支持DSP C66x的
总的来说,我想找类似于第3种的库A,是基于opencv,支持DSP C66x的,这样我就能将基于opencv库的代码改写为基于库A的代码(将opencv库里的函数 f 用库A里的等价函数 f' 替换),然后通过CCS编译,再上传到板子上运行
所以,各位大神是否知道有类似的库,是要支持C66x的,如果没有,是否还有其它的解决方案,万望不吝赐教,先谢谢各位了!