This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS中spi flash 测试



使用TI例程测试SPI flash中发现编译的时候遇到一下问题,尝试了好久没有解决,麻烦能够解答一下不胜感激:

**** Build of configuration Debug for project spiflash ****

"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv7/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -O1 -g --include_path="C:/ti/ccsv7/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="/include" --include_path="../../../include" --define=_DEBUG --diag_warning=225 --ptrdiff_size=32 --no_bad_aliases --std_lib_func_defined --asm_listing --obj_directory="/Debug" --preproc_with_compile --preproc_dependency="main.d_raw"  "../main.c"

>> Compilation failure

>> Compilation failure
subdir_rules.mk:9: recipe for target '/Debug/main.obj' failed
"C:\Users\keylock\AppData\Local\Temp\172603", ERROR!  : [E1000] cannot open
                                                                listing file
                                                                /Debug/main.lst:
                                                                No such file or
                                                                directory
"C:\Users\keylock\AppData\Local\Temp\1064810", ERROR!   at EOF: [E1500]
         file access error:  failed to open "/Debug/main.obj" for writing
"C:\Users\keylock\AppData\Local\Temp\1064810", ERROR!  : [E1000] Failed to write
                                                                 object file :
                                                                 /Debug/main.obj
gmake: *** [/Debug/main.obj] Error 1
'Building file: ../spiflash.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv7/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -O1 -g --include_path="C:/ti/ccsv7/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="/include" --include_path="../../../include" --define=_DEBUG --diag_warning=225 --ptrdiff_size=32 --no_bad_aliases --std_lib_func_defined --asm_listing --obj_directory="/Debug" --preproc_with_compile --preproc_dependency="spiflash.d_raw"  "../spiflash.c"

>> Compilation failure

>> Compilation failure
subdir_rules.mk:16: recipe for target '/Debug/spiflash.obj' failed
"../spiflash.c", line 53: warning: integer conversion resulted in a change of sign
"../spiflash.c", line 172: warning: shift count is too large
"../spiflash.c", line 183: warning: shift count is too large
"../spiflash.c", line 229: warning: shift count is too large
"C:\Users\keylock\AppData\Local\Temp\159123", ERROR!  : [E1000] cannot open
                                                                listing file
                                                                /Debug/spiflash.lst:
                                                                No such file or
                                                                directory
"C:\Users\keylock\AppData\Local\Temp\0958410", ERROR!   at EOF: [E1500]
         file access error:  failed to open "/Debug/spiflash.obj" for writing
"C:\Users\keylock\AppData\Local\Temp\0958410", ERROR!  : [E1000] Failed to write
                                                                 object file :
                                                                 /Debug/spiflash.obj
'Building file: ../spiflash_test.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv7/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -O1 -g --include_path="C:/ti/ccsv7/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="/include" --include_path="../../../include" --define=_DEBUG --diag_warning=225 --ptrdiff_size=32 --no_bad_aliases --std_lib_func_defined --asm_listing --obj_directory="/Debug" --preproc_with_compile --preproc_dependency="spiflash_test.d_raw"  "../spiflash_test.c"

>> Compilation failure

>> Compilation failure
subdir_rules.mk:23: recipe for target '/Debug/spiflash_test.obj' failed
gmake: *** [/Debug/spiflash.obj] Error 1
"C:\Users\keylock\AppData\Local\Temp\189643", ERROR!  : [E1000] cannot open
                                                                listing file
                                                                /Debug/spiflash_test.lst:
                                                                No such file or
                                                                directory
"C:\Users\keylock\AppData\Local\Temp\1373610", ERROR!   at EOF: [E1500]
         file access error:  failed to open "/Debug/spiflash_test.obj" for
           writing
"C:\Users\keylock\AppData\Local\Temp\1373610", ERROR!  : [E1000] Failed to write
                                                                 object file :
                                                                 /Debug/spiflash_test.obj
gmake: *** [/Debug/spiflash_test.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****