This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 bootset 问题:IBL SPI nor flash GPIO 设置



Hello,

目前正在用C6678 开发项目,硬件电路处在开发阶段。有一些关于 boot set的问题:

目前我们采用IBL的 SPI nor flash 启动,GPIO0~15 对boot 进行设置。

Boot Device 通过GPIO1~3 设置:应该是具体的IBL之后的boot device,而不是IBL(IBL代码在EEPROM中,I2C接口),也就是说SPI nor flash启动模式,GPIO3~1应该设置成110,而不是101?

我的理解正确与否?

非常感谢!

BRS,

Meng