This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6672 内核CVDD 及VCC1V0 电压 对应正常工作电流分别是多少比较合适?



Hello 您好,

1)

参考了C6678原理图,所描述的内核电压, CVDD @8A,VCC1V0@5A,这是对C6678八个核所对应电路,分别是8A(CVDD)和 5A(VCC1V0)。

如果采用C6672(两个C66X内核),CVDD 和 VCC1V0 所对应的电流分别对应值多少最为合适,主要需要考虑功耗,不能太高。

2)

如果对CVDD 和 VCC1V0都选3A,是否可以保证C6672 内核可以正常工作?

非常感谢!BRS,

Meng