This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi, 請教一下有關AM3352使用上問題:
按照规格书描述
AM335X会访问4个sector ,但去读flash时,发现,只有读第一个512byte sector,并没有继续读
另外,我们遇到的问题,表现为上电后AM335X不能启动NOR Flash里面的Boot 和 App。
初步分析,在上电后AM335X访问NOR Flash时,用逻辑分析仪抓取到的数据,
可以看出,ROM_CODE在发送读Nor_flash 读命令"0x03"时,norflash设备已回复相应数据,即Size:0xB824,Destination:0x402f0400(即为片内的109K的SRAM),
从 0x6C, 0x00, 0x9F, 0xE5往后的(512字节 - Szie(4字节) - Destination(4字节) = 508字节为固件的内容),但固件远不止508字节,此后A8读完这个512字节的sector后再也没有发送读数据动作
按照正常会将以读取的地址为开头的内容(Boot 和 App)拷贝到AM335X,然后起Boot,但实际并没有,请问后续可以如何确认和分析?
谢谢