附《Sitara Uniflash Flash Programming with Linux》的链接:
processors.wiki.ti.com/.../Sitara_Uniflash_Flash_Programming_with_Linux
我按照教程操作,希望实现从usb0启动内核,但是文档《Sitara Uniflash Flash Programming with Linux》中的一些必要链接打不开:
“Build SPL (also called MLO) and U-Boot for Flashing"
- AM335x - [U-Boot Patch to Add TFTP Boot Configurations]
“Download and Install RAM Filesystem”
- Download the tiny flasher filesystem.
另外,请问有人做过将openwrt从am335x的usb0启动的工作吗?能否给些指导呢?谢谢。