This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

weston启动报错 [23:09:25.219] fatal: failed to create compositor backend



J6 entry芯片,用的是3.03的SDK

启动weston是报错,log如下:

Date: 2017-12-27 UTC
[23:09:24.092] weston 1.9.0
http://wayland.freedesktop.org
Bug reports to: bugs.freedesktop.org/enter_bug.cgi
Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for the official release (2015-09-21 18:11:26 -0700)
[23:09:24.093] OS: Linu[ 100.031773] cyttsp6_i2c_adapter 4-0024: cyttsp6_wakeup: WAKEUP CYTTSP gpio=58 r=0
x, 4.4.84-dirty, #121 SMP PREEMPT Mon Feb 26 11:35:43 CST 2018, armv7l
[23:09:24.093] Using config file '/etc//weston.ini'
[23:09:24.093] Loading module '/usr/lib/weston/drm-backend.so'
[23:09:24.097] Output repaint window is 7 ms maximum.
[23:09:24.097] initializing drm backend
[23:09:24.104] using /dev/dri/card0
[23:09:24.104] Loading module '/usr/lib/weston/gl-renderer.so'
loaded module : gbm_pvr.so
found valid GBM backend : gbm_pvr.so
[23:09:24.111] warning: either no EGL_EXT_platform_base support or specific platform support; falling back to eglGetDisplay.
[23:09:24.119] warning: EGL_EXT_buffer_age not supported. Performance could be affected.
[23:09:24.119] Retrieving EGL client extension string failed.
[ 100.557636] cyttsp6_i2c_adapter 4-0024: _cyttsp6_awake_device_from_deep_sleep: Queueing startup
[ 100.566773] cyttsp6_i2c_adapter 4-0024: _cyttsp6_queue_startup: cyttsp6_startup queued
[ 100.687428] cyttsp6_i2c_adapter 4-0024: cyttsp6_xres: RESET CYTTSP gpio=60 r=0
[ 100.834426] cyttsp6_i2c_adapter 4-0024: cyttsp6_si_get_test_data_: PANEL TEST Status=0 codel=1A
[ 100.850718] cyttsp6_i2c_adapter 4-0024: cyttsp6_si_get_test_data_: SCANNING is ENABLED codel=1A
[ 100.889597] cyttsp6_i2c_adapter 4-0024: TTSP Protocol Version is 2.7
[ 100.986545] cyttsp6_i2c_adapter 4-0024: cyttsp6_startup_: cyttsp6_exit startup rc=0...
[23:09:25.093] input device 'cyttsp6_mt', /dev/input/event0 is tagged by udev as: Touchscreen
[23:09:25.093] input device 'cyttsp6_mt', /dev/input/event0 is a touch device
[23:09:25.093] No currently active connector found.
[23:09:25.093] failed to create output for /sys/devices/platform/omapdrm.0/drm/card0
[23:09:25.219] fatal: failed to create compositor backend
root@dra7xx-evm:~#