This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6655使用88E1112的问题



诸位前辈:

    我仿照TI提供的开发板(6657),使用C6655和88E1112构成千兆网电路。

    1)使用100M网线,88E1112自适应成100M,PC和我的C6655可以通信。

    2)使用1000M网线,8831112自适应成1000M,采用和1)里面同样的程序,但PC和C6655无法通信。C6655发数据,PC上用网络抓包抓不到任何数据。

    3)使用1000M网线,使用TI提供的开发板(6657),采用1)里面同样的程序,PC和C6655可以通信。

    在2)的过程中,RJ45的灯显示1000M正常,PC端网络显示1000M正常,C6655寄存器自适应和PHY协商显示10000M正常,数据发送时,C6655寄存器显示发包正常。而PC就是抓不到数据。

    为什么我在2)的情况下,无法进行PC和C6655通信。拜求诸位前辈指点。