This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在linux 14.04虚拟机安装 CCS7.4.0.00015_linux-x64报错的问题

Other Parts Discussed in Thread: CCSTUDIO

RT

提示了三次报出的错误是installing com.bh.ccstudio.emulation.linux...

里面的log是到了emupack这里 

Error running /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install: stop: Unknown job: udev

安装到这一步的时候,弹出对话框,点击OK之后 在抱一个窗口错误,就歇菜了。没法继续安装了

求助...

  • 以下是尽量补全的错误log部分
    [21:07:31] DEBUG_x64: Changing File Permissions 755 (common/uscif, emulation/drivers, emulation/Blackhawk/Install)
    LINUX
    [21:07:31] DEBUG: USCIF.OUT exists or BHUSCIF.OUT does not exist.
    [21:07:31] DEBUG: BHUSCIF.OUT does not exist to clean up.
    Creating Uninstaller
    Creating uninstaller 25%
    Creating uninstaller 50%
    Creating uninstaller 75%
    Creating uninstaller 100%
    Installation completed
    LINUX
    [21:07:32] DEBUG: Changing File Permissions 755 (uninstallers: /opt/ti/ccsv7/uninstallers/{uninstall_bh_emupack})
    [21:07:32] DEBUG: Changing File Permissions 666 (log file: /tmp/bitrock_installer_18305.log)
    [21:07:32] DEBUG: Running script to install device driver RULES file.
    Executing /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install
    Script exit code: 1

    Script output:
    bh usb560 installation completed successfully. Some versions of Linux
    require a reboot in order for the driver to function properly. For other
    versions restarting udev is sufficient. Restarting udev now ...
    ERROR: failed to restart udev, reboot required

    Script stderr:
    stop: Unknown job: udev
    start: Unknown job: udev

    Error running /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install: stop: Unknown job: udev
    start: Unknown job: udev
    Problem running post-install step. Installation may not complete correctly
    Error running /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install: stop: Unknown job: udev
    start: Unknown job: udev
    179,1 97%

  • 请问是用root/sudo安装的吗? 请试试用root权限重装一下,安装目录要清空。
    apt-get update
  • 的确是的 昨天弄了一天都没有弄好,我今天把虚拟机卸载了重新装了个最新版本的,然后ubuntu 那个镜像不要了重新下了一个16.04

    今天貌似就可以了

    虽然装了但是却不知道昨天装的过程中出错的原因到底是 安装的库文件不对还是换了新版本。

    可能的原因1.昨天是在14.04.5的ubuntu下装的

    2.昨天是在低版本的虚拟机装的

    3.昨天安装的库文件一大堆,

    apt-get update​ 
    apt-get install libc6:i386 libx11-6:i386 libasound2:i386 libatk1.0-0:i386 libcairo2:i386 libcups2:i386 libdbus-glib-1-2:i386 libgconf-2-4:i386 libgcrypt20:i386 libgdk-pixbuf2.0-0:i386 libgtk-3-0:i386 libice6:i386 libncurses5:i386 libsm6:i386 liborbit2:i386 libudev1:i386 libusb-0.1-4:i386 libstdc++6:i386 libxt6:i386 libxtst6:i386 libgnomeui-0:i386 libusb-1.0-0-dev:i386 libcanberra-gtk-module:i386 gtk2-engines-murrine:i386 unzip

    以及apt-get install libnss3:i386 libnss3-1d:i386 libnss3-nssdb:i386

    而今天按ti的就执行了俩:apt-get update  apt-get install libc6:i386

    因此,不知道昨天出错的具体原因了 我还是希望ti的技术大大能够给我解答

  • 请问你是在线安装的吗?
  • 应该是Ubuntu14.04里面的库比较老不匹配导致的。
  • 在Windows上安装也会出现类似的错误