This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

beagleboard-xm REVC uboot出现的问题

Expert 1041 points


U-Boot 2010.06 (Oct 29 2012 - 22:34:32)

OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C:   ready
DRAM:  384 MiB
NAND:  HW ECC [Kernel/FS layout] selected
0 MiB
*** Warning - bad CRC or NAND, using default environment

In:    serial
Out:   serial
Err:   serial
Beagle xM Rev A
Die ID #037600029ff80000016849a902025014
Hit any key to stop autoboot:  0
uboot运行起来的结果是384M,实际是512M的,我用自带的这个uboot镜像可以出来512,但是用dvsdk4.0.3编译出的beagle uboot读出的dram为384,想咨询一下这个数值产生错误的原因。因为内存都错误了所以内核起不来。