This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H Rev40 uboot tftp



MCSDK 3.x User Guide

Loading and Running Linux Kernel using tftp with NFS file system

>setenv serverip 192.168.1.10
>setenv tftp_root release
>setenv nfs_root export/release
>setenv boot net
>saveenv
>boot

我按照手册上面的设置进行tftp下载内核,nfs挂载文件系统,遇到如下问题:

设置好bootfile :    setenv  bootfile   uImage,  当boot后,总是出现错误:

K2HK EVM # boot
BOOTP broadcast 1
BOOTP broadcast 2
*** Unhandled DHCP Option in OFFER/ACK: 52
*** Unhandled DHCP Option in OFFER/ACK: 52
DHCP client bound to address 192.168.1.100
Using K2HK_EMAC device
TFTP from server 192.168.1.192; our IP address is 192.168.1.100
Filename '�'.
Load address: 0x87000000

这时再查看bootfile,  printenv bootfile:

bootfile=�