CCS6.0怎么烧录程序到C5515的外部SPI Flash?
在http://processors.wiki.ti.com/index.php/C5515_Boot-Image_Programmer#Software_Tools_Checklist只有简单的描述,
How to program a boot image onto C5515 EVM
Once a boot image (*.bin) is generated, customers can burn the boot image into the NOR Flash, NAND Flash, 16-bit SPI EEPROM, I2C EEPROM, and MMC/SD card, on the C5515 EVM through a utility called programmer that runs on C5515 using an emulator with Code Composer Studio™ software.
而且不适用于CCS6.0。
请问编译成功后,得到.out文件,如何将其烧录到外部SPI FLASH上,还需要什么步骤和软件工具?
谢谢大家的帮助!