This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 dvrrdk 采集 XGA视频信号



我想用dvrrdk2.80 采集xga信号,板子重新设计了,视频解码芯片使用adv7181,

但是没有驱动程序,怎么把其他解码片子的驱动加到rdk里呢?

看了rdk的capture link是不是要对capture_drv 进行修改啊?

  • 视频AD/DA芯片驱动可以单独加载,也可以编入内核。如果想加入RDK,可以参考

    DVRRDK_03.00.01.03\ti_tools\hdvpss\hdvpss_01_00_01_37_patched\packages\ti\psp\devices

    下程序包,以上路径为我的RDK包,你找对应RDK2.80的就OK了。