This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP5509A使用DMA乒乓缓存从McBSP0读取AIC23的数据进入不了中断

Other Parts Discussed in Thread: TMS320VC5509A

/******************************************************************************/
/* this program is that the codec is controled by the I2C and Mcbsp 	      */
/*----------------------------------------------------------------------------*/

#include <csl.h>
#include <csl_i2c.h>
#include <stdio.h>
#include <csl_pll.h>
#include <csl_mcbsp.h>
#include <csl_irq.h>
#include <math.h>
#include <function.h>
#include <csl_dma.h>

#define State_Signal_Process 1

/* Define transmit and receive buffers */
int pingrcv[FRAME_LENGTH];
int pongrcv[FRAME_LENGTH];
int pingxmt[FRAME_LENGTH];
int pongxmt[FRAME_LENGTH];
int Leftchannel_Buffer[FRAME_LENGTH];
int Rightchannel_Buffer[FRAME_LENGTH];

int xfreebuf;
int rfreebuf;

int State_Work=0;

//volatile Uint16 transferComplete = FALSE;
Uint16 old_intm;

Uint16 rcvEventId;
Uint16 xmtEventId;

//---------Function prototypes---------
/* Reference start of interrupt vector table */
/* This symbol is defined in file, vectors.s55 */
extern void VECSTART(void);

void delay(Uint32 k);

void I2C_Set_Init();
void McBSP_Set_Init();
void DMA_DataTransfer_Init();
void Signal_Process();

/* Protoype for interrupt functions */
interrupt void dmaXmtIsr(void);
interrupt void dmaRcvIsr(void);


/*锁相环的设置*/
PLL_Config  myConfig      = {
  0,    //IAI: the PLL locks using the same process that was underway
                //before the idle mode was entered
  1,    //IOB: If the PLL indicates a break in the phase lock,
                //it switches to its bypass mode and restarts the PLL phase-locking
                //sequence
  12,    //PLL multiply value; multiply 24 times
  1             //Divide by 2 PLL divide value; it can be either PLL divide value
                //(when PLL is enabled), or Bypass-mode divide value
                //(PLL in bypass mode, if PLL multiply value is set to 1)
};

/*McBSP set,we use mcbsp1 to send and recieve the data between DSP and AIC23*/
MCBSP_Config Mcbsp1Config= {
	MCBSP_SPCR1_RMK(
    MCBSP_SPCR1_DLB_OFF,                   /* DLB    = 0,禁止自闭环方式 */
    MCBSP_SPCR1_RJUST_LZF,                 /* RJUST  = 2 left justify the data and zero fill LSBS */
    MCBSP_SPCR1_CLKSTP_DISABLE,            /* CLKSTP = 0 Clock stop mode disable */
    MCBSP_SPCR1_DXENA_ON,                  /* DXENA  = 1 DX delay enabler on */
    MCBSP_SPCR1_ABIS_DISABLE,              /* ABIS   = 0 reserved always write 0*/
    MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 sends a receive INT request to CPU when the RRDY bit
                                            change from 0 to 1, indicating that receive data is ready to be read*/
    0,                                     /* RSYNCER = 0 receive frame-sync error bit, no error*/
    MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 reset the receiver*/
       ),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 free run bit, The McBSP transmit and receive clocks are affected as determined by the SOFT bit*/
    MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 Soft stop bit, Hard stop*/
   MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 Frame-sync logic reset bit*/
    MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 Sample rate generator reset bit */
    MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 transmit interrupt mode bits XRDY bit changes from 0 to1 */
    0,                                     /* XSYNCERR = N/A transmit frame-sync error bit, no error*/
    MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 transmit ready bit, not ready*/
       //注意:开始一定要设置为disable,否则不能设置它的寄存器,全部为默认值,导致不能正常接收,
       //在程序调用C库函数mcbspstart时会在设为1,McBSP便退出reset状态开始工作
   ),
    /*单数据相,接受数据长度为16位,每相2个数据*/
  MCBSP_RCR1_RMK(
    MCBSP_RCR1_RFRLEN1_OF(1),              /* RFRLEN1 = 1 Receive frame length 1 bits(1 to 128 words),Frame length=(RFRLEN1+1)words*/
      MCBSP_RCR1_RWDLEN1_16BIT               /* RWDLEN1 = 2 Receive word length 1 bits, 16bit*/
  ),
 MCBSP_RCR2_RMK(
   MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 Receive phase number bit, single-phase frame*/
    MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 */
    MCBSP_RCR2_RWDLEN2_8BIT,               /* RWDLEN2 = 0 */
    MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 receive companding mode bits, 0, no companding,MSB received first*/
    MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0 Receive frame-sync ignore bit, 1, frame-sync detect */
    MCBSP_RCR2_RDATDLY_1BIT                /* RDATDLY = 1 Receive data delay bits, 1-bit data delay*/
    ),
   MCBSP_XCR1_RMK(
    MCBSP_XCR1_XFRLEN1_OF(1),              /* XFRLEN1 = 1 Transmit frame length 1(1 to 128 words),Frame length=(XFRLEN1+1)words */
    MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 2 Transmit word length 1.16bit*/
   ),
 MCBSP_XCR2_RMK(
    MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 Transmit phase number bit, single-phase frame*/
    MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT,               /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 Transmit companding mode bits, 0, no companding,MSB received first*/
    MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 Transmit frame-sync ignore bit, 1, frame-sync detect */
    MCBSP_XCR2_XDATDLY_1BIT                /* XDATDLY = 1 Transmit data delay bits, 1-bit data delay*/
  ),
 MCBSP_SRGR1_DEFAULT,                      /*(0x0001u)FWID=0,CLKGDV=1 */
 MCBSP_SRGR2_DEFAULT,                      /*(0x2000u)CLKSM=1,Sample rate generator input clock mode bit */
 MCBSP_MCR1_DEFAULT,
 MCBSP_MCR2_DEFAULT,
 MCBSP_PCR_RMK(
  MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0 The McBSP remains active when the PERIPH domain is idled */
   MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0 Transmit I/O enable bit, CLKX,FSX,DX,CLKS pins are serial port pins*/
   MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0 Receive I/O enable bit, CLKR,FSR,DR,CLKS pins are serial port pins*/
   MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0 Transmit frame-sync mode bit,0:transmit fram-sync is supplied by an external source via the FSX pin*/
   MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0 Receive frame-sync mode bit,0:transmit fram-sync is supplied by an external source via the FSR pin*/
   0,                                      /* DXSTAT = N/A   */
   MCBSP_PCR_CLKXM_INPUT,                  /* CLKXM    = 0 Transmit clock mode bit*/
   MCBSP_PCR_CLKRM_INPUT,                  /* CLKRM    = 0 Receive clock mode bit*/
   MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0 Sample rate generator input clock mode bit,used with CLKSM to select the input clock*/
   MCBSP_PCR_FSXP_ACTIVEHIGH,              /* FSXP     = 0 Transmit frame-sync polarity bit, 0,transmit frame-sync pulses are active high*/
   MCBSP_PCR_FSRP_ACTIVEHIGH,              /* FSRP     = 1 Receive frame-sync polarity bit, 0,receive frame-sync pulses are active high*/
   MCBSP_PCR_CLKXP_FALLING,                /* CLKXP    = 1 Transmit clock polarity bit,1,transmit data is driven on the rising edge of CLKX */
   MCBSP_PCR_CLKRP_RISING                  /* CLKRP    = 1 Receive clock polarity bit*/
 ),
 MCBSP_RCERA_DEFAULT,
 MCBSP_RCERB_DEFAULT,
 MCBSP_RCERC_DEFAULT,
 MCBSP_RCERD_DEFAULT,
 MCBSP_RCERE_DEFAULT,
 MCBSP_RCERF_DEFAULT,
 MCBSP_RCERG_DEFAULT,
 MCBSP_RCERH_DEFAULT,
 MCBSP_XCERA_DEFAULT,
 MCBSP_XCERB_DEFAULT,
 MCBSP_XCERC_DEFAULT,
 MCBSP_XCERD_DEFAULT,
 MCBSP_XCERE_DEFAULT,
 MCBSP_XCERF_DEFAULT,
 MCBSP_XCERG_DEFAULT,
 MCBSP_XCERH_DEFAULT
};

DMA_Config dmaRcvConfig = {
		DMA_DMACSDP_RMK(
				DMA_DMACSDP_DSTBEN_NOBURST,/* DSTBEN = 0 */
				DMA_DMACSDP_DSTPACK_OFF,/* DSTPACK = 0 */
				DMA_DMACSDP_DST_DARAM,/* DST = 1 */
				DMA_DMACSDP_SRCBEN_NOBURST,/* SRCBEN = 0 */
				DMA_DMACSDP_SRCPACK_OFF,/* SRCPACK = 0 */
				DMA_DMACSDP_SRC_PERIPH,/* SRC = 3 */
				DMA_DMACSDP_DATATYPE_16BIT/* DATATYPE = 1 */
		),/* DMACSDP源和目标参数寄存器 */
		DMA_DMACCR_RMK(
				DMA_DMACCR_DSTAMODE_POSTINC,/* DSTAMODE = 1 */
				DMA_DMACCR_SRCAMODE_CONST,/* SRCAMODE = 0  */
				DMA_DMACCR_ENDPROG_ON,/* ENDPROG = 1 */
				DMA_DMACCR_REPEAT_OFF,/* REPEAT = 0*/
				DMA_DMACCR_AUTOINIT_OFF,/* AUTOINIT = 1 */
				DMA_DMACCR_EN_STOP,/* EN = 0 */
				DMA_DMACCR_PRIO_HI,/* PRIO = 1 */
				DMA_DMACCR_FS_DISABLE,/* FS = 1   */
				DMA_DMACCR_SYNC_REVT0/* SYNC = 5 DMA_DMACCR_SYNC_NONE*/
		),/* DMACCR 通道控制寄存器 */
		DMA_DMACICR_RMK(
				DMA_DMACICR_BLOCKIE_OFF,/* BLOCKIE = 0 */
				DMA_DMACICR_LASTIE_OFF,/* LASTIE = 0 */
				DMA_DMACICR_FRAMEIE_ON,/* FRAMEIE = 1 */
				DMA_DMACICR_FIRSTHALFIE_OFF,/* FIRSTHALFIE = 0 */
				DMA_DMACICR_DROPIE_OFF,/* DROPIE = 0 */
				DMA_DMACICR_TIMEOUTIE_OFF/* TIMEOUTIE = 0 */
		), /* DMACICR 中断控制寄存器*/
		(DMA_AdrPtr)(MCBSP_ADDR(DRR10)), /* DMACSSAL 源起始地址低位寄存器*/
		0, /* DMACSSAU 源起始地址高位寄存器*/
		(DMA_AdrPtr)&pingrcv, /* DMACDSAL  目标起始地址低位寄存器*/
		0, /* DMACDSAU 目标起始地址高位寄存器*/
		FRAME_LENGTH, /* DMACEN 要素个数寄存器,装入每帧的要素数*/
		1, /* DMACFN 帧数寄存器,装入每块的帧数*/
		0, /* DMACFI 帧索引寄存器*/
		0 /* DMACEI 要素索引寄存器*/
};

DMA_Config  dmaXmtConfig = {
  DMA_DMACSDP_RMK(
	DMA_DMACSDP_DSTBEN_NOBURST,    //Destination burst :-不使用突发
    DMA_DMACSDP_DSTPACK_OFF,       //Destination packing :-目标口禁止打包
    DMA_DMACSDP_DST_PERIPH,        //Destination selection :-接收的目标口是外设mcbsp
    DMA_DMACSDP_SRCBEN_NOBURST,    //Source burst :-源突发禁止
    DMA_DMACSDP_SRCPACK_OFF,       //Source packing :-源口禁止打包
    DMA_DMACSDP_SRC_DARAM,        //Source selection :源口为DARAM
    DMA_DMACSDP_DATATYPE_16BIT    //Data type :-设置数据类型16bit字长
  ),                                       /* DMACSDP  源与目标参数寄存器 */
  DMA_DMACCR_RMK(
    DMA_DMACCR_DSTAMODE_CONST,    //Destination address mode :-目标口地址为恒定地址
    DMA_DMACCR_SRCAMODE_POSTINC,  //Source address mode :-自动执行后增量(由于本程序中数据类型是16bit,所以+2)
    DMA_DMACCR_ENDPROG_ON,        //End of programmation bit :-
    DMA_DMACCR_REPEAT_OFF,
	DMA_DMACCR_AUTOINIT_OFF,       //Auto initialization bit :-
    DMA_DMACCR_EN_STOP,           //Channel enable :-设置时先关闭通道
	DMA_DMACCR_PRIO_HI,          //Channel priority :-设置为低优先级
	DMA_DMACCR_FS_DISABLE,        //Frame/Element Sync :-单元事件同步
    DMA_DMACCR_SYNC_XEVT0         //Synchronization control :-McBSP1 Transmit Event(XEVT1)
  ),                                       /* DMACCR 通道控制寄存器   */
  DMA_DMACICR_RMK(
	DMA_DMACICR_BLOCKIE_OFF,       //Whole block interrupt enable :-块传输完成后中断使能
    DMA_DMACICR_LASTIE_OFF,       //Last frame interrupt enable :-
	DMA_DMACICR_FRAMEIE_ON,       //Whole frame interrupt enable :-
    DMA_DMACICR_FIRSTHALFIE_OFF,  //Half frame interrupt enable :-
    DMA_DMACICR_DROPIE_OFF,       //Sync. event drop interrupt enable :-
    DMA_DMACICR_TIMEOUTIE_OFF     //Time out interrupt enable :-
  ),                                       /* DMACICR 中断控制寄存器 */
    (DMA_AdrPtr)&pingxmt[0],                   /* DMACSSAL 源地址低位*/
    0,                                     /* DMACSSAU 源地址高位 */
    (DMA_AdrPtr)(MCBSP_ADDR(DXR10)),       /* DMACDSAL 目的地址低位*/
    0,                                     /* DMACDSAU 目的地址高位*/
	FRAME_LENGTH,                                     /* DMACEN   1 帧内数据长度 16*2 两个数据一个帧*/
	1,                                     /* DMACFN  帧数大小  */
    0,                                     /* DMACFI   */
    0                                      /* DMACEI   */
};

/* This next struct shows how to use the I2C API */
/* Create and initialize an I2C initialization structure */
I2C_Setup I2Cinit = {
        0,              /* 7 bit address mode */
        0,         /* own address - don't care if master */
        84,            /* clkout value (Mhz)  */
        50,            /* a number between 10 and 400*/
        0,              /* number of bits/byte to be received or transmitted (8)*/
        0,              /* DLB mode on*/
        1               /* FREE mode of operation on*/
};

/*数字音频接口格式设置
AIC23为主模式,数据为DSP模式,数据长度16位*/
Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
/*AIC23的波特率设置,采样率为44.1K*/
Uint16 sample_rate_control[2] = {0x10,0x20};
/*AIC23寄存器复位*/
Uint16 reset[2] ={0x1e,0x00};
/*AIC23节电方式设置,所有部分均所与工作状态*/
Uint16 power_down_control[2] ={0x0c,0x01};
/*AIC23模拟音频的控制
DAC使能,ADC输入选择为MIC*/
Uint16 analog_aduio_path_control[2] ={0x08,0x15};
/*AIC23数字音频通路的控制*/
Uint16 digital_audio_path_control[2] ={0x0a,0x05};
/*AIC23数字接口的激活*/
Uint16 digital_interface_activation[2] ={0x12,0x01};
/*AIC23左通路音频调节*/
Uint16 left_line_input_volume_control[2] ={0x00,0x00};
/*AIC23右通路音频调节*/
Uint16 right_line_input_volume_control[2] ={0x02,0x00};
/*AIC23耳机左通路音频调节*/
Uint16 left_headphone_volume_control[2] ={0x05,0x79};
/*AIC23耳机右通路音频调节*/
Uint16 right_headphone_volume_control[2] = {0x07,0x79};

/*定义McBSP的句柄*/
MCBSP_Handle hMcbsp;
MCBSP_Config Mcbsptest;

I2C_Config testI2C;

/*定义DMA的句柄*/
DMA_Handle hDmaRcv;
DMA_Handle hDmaXmt;

void main(void)
{
    /* Initialize CSL library - This is REQUIRED !!! */
    /*初始化CSL库*/
    CSL_init();

	/*设置系统的运行速度为140MHz*/
    PLL_config(&myConfig);

    /*初始化I2C */
	I2C_Set_Init();

	/*初始化McBSP */
	McBSP_Set_Init();

	/*初始化DMA */
	DMA_DataTransfer_Init();

	while(TRUE){
		if(State_Work==State_Signal_Process){
			Signal_Process();
			State_Work=0;
		}
	}
}

void delay(Uint32 k){
   while(k--);
}

void I2C_Set_Init(){

    /* Initialize I2C, using parameters in init structure */
    /*初始化I2C的格式*/
//	I2C_config(&Config);
//	I2C_start();

//	I2C_getConfig(&Config1);
	/*I2C is undet reset*/
	I2C_RSET(I2CMDR,0);

	/*设置预分频寄存器,I2C的mode clock is 10MHz*/
	delay(100);
	I2C_RSET(I2CSAR,0x001A);

	I2C_RSET(I2CMDR,0x0620);

    I2C_setup(&I2Cinit);

  	/*设置I2C的Mater clock*/
	I2C_RSET(I2CCLKL,100);

	I2C_RSET(I2CCLKH,100);

    I2C_getConfig(&testI2C);

    /*reset AIC23*/
    i2c_status = I2C_write( reset,          //pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver--master
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    		            );
	delay(1000);

    /*设置AIC23各部分均工作*/
    i2c_status = I2C_write( power_down_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    		            );

	/*设置AIC23的数字接口*/
	i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	               	);

	 /*设置AIC23模拟通路*/
	i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    		            );

	/*设置数字通路*/
	i2c_status = I2C_write( digital_audio_path_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	              	);

	/*设置AIC23的采样率*/
	i2c_status = I2C_write( sample_rate_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	                );

	/*设置耳机音量*/
	i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	                );

	i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	                );

	/*设置Line输入的音量*/
	i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	                );

	i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array
	    	                2,				//length of data to be transmitted
	    	                1,				//master or slaver
	    	                CODEC_ADDR,	    //slave address to transmit to
	    	                1,				//transfer mode of operation
	    	                30000			//time out for bus busy
	    	                );

	/*启动AIC23*/
	i2c_status = I2C_write( digital_interface_activation,//pointer to data array
	    	   2,				//length of data to be transmitted
	    	   1,				//master or slaver
	    	   CODEC_ADDR,	    //slave address to transmit to
	    	   1,				//transfer mode of operation
	    	   30000			//time out for bus busy
	    	   );

}


void McBSP_Set_Init(){

	/* Open MCBSP Port 1 and set registers to their power on defaults */
	hMcbsp = MCBSP_open(MCBSP_PORT0,MCBSP_OPEN_RESET);

	/* Write values from configuration structure to MCBSP control regs */
	MCBSP_config(hMcbsp,&Mcbsp1Config);

	/* Start Sample Rate Generator and Enable Frame Sync */
	MCBSP_start(hMcbsp,
		        MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
		        0x300u);

	/* Take MCBSP transmit and receive out of reset */
	MCBSP_start(hMcbsp,
		        MCBSP_XMIT_START | MCBSP_RCV_START,
		        0u);

//	MCBSP_start(hMcbsp,
//	            MCBSP_RCV_START | MCBSP_XMIT_START,
//	            0);

	MCBSP_getConfig(hMcbsp,&Mcbsptest);

}

void DMA_DataTransfer_Init()
{
	Uint16 srcAddrHi, srcAddrLo;
	Uint16 dstAddrHi, dstAddrLo;

	int i;
	//乒乓数组初始化
	for(i=0;i<FRAME_LENGTH;i++){
		pingrcv[i] = 0;
		pongrcv[i] = 0;
		pingxmt[i] = 0;
		pongxmt[i] = 0;
	}

	xfreebuf = xpongbuf;
	rfreebuf = rpongbuf;

	/* Set IVPD/IPVH to start of interrupt vector table */
	IRQ_setVecs((Uint32)(&VECSTART));

	/* By default, the TMS320C55xx compiler assigns all data symbols word */
	/* addresses. The DMA however, expects all addresses to be byte       */
	/* addresses. Therefore, we must shift the address by 2 in order to   */
	/* change the word address to a byte address for the DMA transfer.
	* MCBSP_ADDR()函数用来取址,DRR11是数据接收寄存器,即DMA寄存器从此接收数据
	* 表示DMA从MCBSP传数据到pingrcv*/
    srcAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(&pingrcv)) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(&pingrcv)) << 1) & 0xFFFFu;

    dmaRcvConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaRcvConfig.dmacssau = srcAddrHi;
    dmaRcvConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaRcvConfig.dmacdsau = dstAddrHi;

	/* 表示DMA从pingxmt传数据到MCBSP*/
    srcAddrHi = (Uint16)(((Uint32)(&pingxmt[0])) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(&pingxmt[0])) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) << 1) & 0xFFFFu;

    dmaXmtConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaXmtConfig.dmacssau = srcAddrHi;
    dmaXmtConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaXmtConfig.dmacdsau = dstAddrHi;

	/* Open DMA channels 4 & 5 and set regs to power on defaults */
	hDmaRcv = DMA_open(DMA_CHA4,DMA_OPEN_RESET);
	hDmaXmt = DMA_open(DMA_CHA5,DMA_OPEN_RESET);

	/* Get interrupt event associated with DMA receive and transmit */
	xmtEventId = DMA_getEventId(hDmaXmt);
	rcvEventId = DMA_getEventId(hDmaRcv);

	/* Temporarily disable interrupts and clear any pending      加上去的*/
	/* interrupts for MCBSP transmit */
	old_intm = IRQ_globalDisable();

	/* Clear any pending interrupts for DMA channels */
	IRQ_clear(xmtEventId);
	IRQ_clear(rcvEventId);

	/* Enable DMA interrupt in IER register */
	IRQ_enable(xmtEventId);
	IRQ_enable(rcvEventId);

	/* Set Interrupt Vector Start Location */
	IRQ_setVecs(0x10000);

	/* Place DMA interrupt service addresses at associate vector
	* 连接两个中断函数*/
	IRQ_plug(xmtEventId,&dmaXmtIsr);
	IRQ_plug(rcvEventId,&dmaRcvIsr);

	/* Write values from configuration structure to DMA control regs */
	DMA_config(hDmaRcv,&dmaRcvConfig);
	DMA_config(hDmaXmt,&dmaXmtConfig);

	/* Enable all maskable interrupts */
	IRQ_globalEnable();

	/* Enable DMA */
	DMA_start(hDmaRcv);
	DMA_start(hDmaXmt);

	/* 获取DMAD的MACCR寄存器ENDPROG字段值,为1表示编程结束。
	*  */
	while(DMA_FGETH(hDmaRcv, DMACCR, ENDPROG));

	/* 表示DMA从pongxmt传数据到pongrcv*/
    dstAddrHi = (Uint16)(((Uint32)(&pongrcv)) >> 15) & 0xFFFFu;
   dstAddrLo = (Uint16)(((Uint32)(&pongrcv)) << 1) & 0xFFFFu;
    dmaRcvConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaRcvConfig.dmacdsau = dstAddrHi;

   srcAddrHi = (Uint16)(((Uint32)(&pongxmt[0])) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(&pongxmt[0])) << 1) & 0xFFFFu;
    dmaXmtConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
   dmaXmtConfig.dmacssau = srcAddrHi;

	/* 赋值DMAD的MACCR寄存器ENDPROG字段,为1表示编程结束。
	*  */
    DMA_FSETH(hDmaRcv, DMACCR, ENDPROG,1);
    DMA_FSETH(hDmaXmt, DMACCR, ENDPROG,1);
}

/*播放声音的中断*/
interrupt void dmaXmtIsr(void) {
	printf("……进入中断   dmaXmtIsr……\n");
    static int * ptr;
    unsigned int ptraddrhi, ptraddrlow;
    /* 赋值DMAD的DMACSR寄存器BLOCK字段,为0表示整块时间没有发生,为1表示整块已经传输完毕,一个中断请求已经发送给CPU。
        *  */
    DMA_FSETH(hDmaXmt,DMACSR,FRAME,0);
    if(xfreebuf == xpingbuf){
        xfreebuf = xpongbuf;
        ptr = pongxmt;
    }else{
        xfreebuf = xpingbuf;
        ptr = pingxmt;
    }
    /* 获取DMAD的MACCR寄存器ENDPROG字段值,为1表示编程结束。
         *  */
    while(DMA_FGETH(hDmaXmt, DMACCR, ENDPROG));
    //修改DMA地址
    ptraddrhi = (unsigned int)(((unsigned long)(ptr)) >> 15) & 0xFFFFu;
    //因为DMA都使用字节地址,所以必须左移一位
    ptraddrlow= (unsigned int)(((unsigned long)(ptr)) << 1) & 0xFFFFu;
    DMA_RSETH(hDmaXmt, DMACSSAU, ptraddrhi);
    DMA_RSETH(hDmaXmt, DMACSSAL, ptraddrlow);
    DMA_FSETH(hDmaXmt, DMACCR, ENDPROG,1);
}

/*接受声音的中断*/
interrupt void dmaRcvIsr(void) {
	printf("……进入中断   dmaRcvIsr……\n");
	static int * ptr;
    unsigned int ptraddrhi, ptraddrlow;
    DMA_FSETH(hDmaRcv,DMACSR,FRAME,0);
    if(rfreebuf == rpingbuf){
    	rfreebuf = rpongbuf;
        ptr = pongrcv;
    }else{
  	   	rfreebuf = rpingbuf;
        ptr = pingrcv;
    }
   while(DMA_FGETH(hDmaRcv, DMACCR, ENDPROG));
    //修改DMA地址
    ptraddrhi = (unsigned int)(((unsigned long)(ptr)) >> 15) & 0xFFFFu;
    //因为DMA都使用字节地址,所以必须左移一位
    ptraddrlow= (unsigned int)(((unsigned long)(ptr)) << 1) & 0xFFFFu;
    DMA_RSETH(hDmaRcv, DMACSSAU, ptraddrhi);
    DMA_RSETH(hDmaRcv, DMACSSAL, ptraddrlow);
    DMA_FSETH(hDmaRcv, DMACCR, ENDPROG,1);
    State_Work = State_Signal_Process;
}

void Signal_Process()
{
	printf("……进入处理函数  Signal_Process……\n");
    Uint16 i,j=0;
    if(rfreebuf == rpongbuf){									//(PingPong == PING)
       for(i=0;i<FRAME_LENGTH;i=i+2){
           Leftchannel_Buffer[j] = pongrcv[i];
           Rightchannel_Buffer[j] = pongrcv[i+1];
           j++;
       }
    }else{
       for(i=0;i<FRAME_LENGTH;i=i+2){
          Leftchannel_Buffer[j] = pingrcv[i];
          Rightchannel_Buffer[j] = pingrcv[i+1];
          j++;
       }
   }
   j = 0;
   if(xfreebuf == xpongbuf){
       for(i=0;i<FRAME_LENGTH;i=i+2){
          pongxmt[i] = Leftchannel_Buffer[j];
          pongxmt[i+1] = Rightchannel_Buffer[j];
          j++;
       }
   }else{
       for(i=0;i<FRAME_LENGTH;i=i+2){
           pingxmt[i] = Leftchannel_Buffer[j];
           pingxmt[i+1] = Rightchannel_Buffer[j];
           j++;
       }
   }
}

/******************************************************************************/
/* End of main.c                                                              */
/******************************************************************************/