This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 encode延时大

目前正在做DM368的项目,前端通过ADV7604将DVI接口视频转为YUV420sp传入368,使用DVSDK中自带的encode示例程序,然后将H264数据通过RTP发送并通过自己编写的上位机软件解码播放,延时大概有200ms。

上位机软件是之前一直在使用的,也同样用在DM8168和海思平台,可以确定的是上位机软件解码及绘制占用时间很小,不超过30ms,所以时间基本就在encode程序里边了,将encode里的capture buffer size和fifo size改小会有一点效果,但不明显。

想请问下,还需要修改那些地方能降低延时,谢谢大神?