Other Parts Discussed in Thread: AM5728
你好,
我们自己做了一个am5728的板子,使用的是emmc型号如下:KLMAG1JENB-B041 16GB, 我们使用的IO电平是3.3V,从cpu的手册上我看到,MMC2是支持4.5标准的,最高支持HS200,由于我们使用的3.3VIO cpu 只能跑在DS mode 24M clock 或者HS mode 48M clock。从emmc flash 芯片来看,它可以支持High-Speed Dual Data Rate e•MMC at 52 MHz - 1.8 V or 3 V I/O, 我现在在dts文件配置时钟为24M 或48M, mmc都不能正确初始化,在发送CMD8时,得到的响应是正确的但是无法读到寄存器内容。具体报错信息可以看下面的trace 。现在不知问题出在哪里,也不知我的理解是否正确?7357.trace.txt5710.KLMxGxJENB-B041(eMMC5.1 1ynm based e_MMC)1.0.pdf