This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

官方DVR RDK中的代码注释疑似错误~! DM8148开发

作为一名新人菜菜,最近在弄DM8148的芯片,一直在看程序,有些地方存在疑惑,请求指教~!谢谢~!

/**
\brief Display Device Parameter
*/
typedef struct VDIS_DEV_PARAM_S
{
UInt32 enable;
/**< Enable/Disable Venc usage */       是不是应该改为   /**< Enable/Disable Vdis usage */   

Demo代码是:

vdisParams.deviceParams[VDIS_DEV_HDCOMP].enable = FALSE;//TRUE; //   

这是 vdis Params变量 结构体类型的定义

/**
\brief Display Sub-system initialization parameters
*/
typedef struct
{
UInt32 numUserChannels;
/**< Number of displays that are active */

UInt32 tiedDevicesMask;
/**< Vencs tied together. This can be a ORed value of
VDIS_VENC_HDMI,
VDIS_VENC_HDCOMP,
VDIS_VENC_DVO2,
VDIS_VENC_SD */

UInt32 enableConfigExtThsFilter;
/**< When FALSE do not configure THS from M3 / McFW side */

UInt32 enableConfigExtVideoEncoder;
/**< When FALSE do not configure Sii9022A from M3 / McFW side */

UInt32 enableEdgeEnhancement;
/**< Enable/Disable edge enhancement */

UInt32 enableLayoutGridDraw;
/**< Enable/Disable Drawing of Layout specific Grids: TRUE/FALSE */

VDIS_DEV_PARAM_S deviceParams[VDIS_DEV_MAX];
/**< Device parameters */

VDIS_MOSAIC_S mosaicParams[VDIS_DEV_MAX];
/**< Initial mosaic for each display device */

UInt32 numChannels;
/**< Number of channel inputs to display device */

UInt32 mosaicLayoutResolution[VDIS_DEV_MAX];
/**< SWMS output Layout Resolution */

Bool enableHdmiControl;
/**< Enables a thread to monitor interface, used to detect TV plug in/plug 
out. */

} VDIS_PARAMS_S;