This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 DSP 和FPGA srio message通信



大神,请教下两个问题。

1. dsp srio速率1.25G,type11模式,自环模式下,每包发送4096字节,发送的包数和中断接收的包数相等。但是每包发送256字节,发送的包数和中断接收的包数不相等,接收丢包,这是什么原因导致的。

2. 和fpga进行message通信,fpga发256字节时,dsp可以收到每包大小256,但是fpga发送4096时,dsp只能接收每包256,接收端配置的单端和多段,配置没问题,如何让dsp也能中断接收每包4096字节。

3. 和fpga进行message通信,fpga发每包256字节时,发送超过70包以上,dsp就出现丢包现象。

请大神指教下,谢谢

  • 大神,你好,请教下问题

    我用的6657,sriomessage模式,和FPGA通信,1.25G,链路连接上后,每包发送256字节,但是全速运行时,FPGA只能抓到前几包,当运行过程中,FPGA重新烧程序,DSP这边也会发送成功,为什么。

    发送4098字节时,速率竟然有200MB/s,完全超出理论速度。

    求大神指点下,谢谢