This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748连接TDS510仿真器错误

Other Parts Discussed in Thread: TMS320C6748

TMS320C6748  仿真器用的是Wintech的TDS510USB2.0

连接的时候出现以下error

Error connecting to the target:
Error 0x80000240/-1146
Fatal Error during: Initialization, OCS,
Invalid data was scanned by the emulation controller.
Verify the board setup to make sure the scan chain is properly
defined.
If the setup is correct, then RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

运行Reset TDS510USB2.0.bat和Probe TDS510USB2.0.bat都没有问题,是什么原因连接不上呢??????