TMS320C6748 仿真器用的是TI的XDS510-USB2.0
连接的时候出现以下error:
Error connecting to the target:
Error 0x80000244/-2131
Fatal Error during: Register, Initialization, OCS,
Cannot access register at 0x00000000
I/O Port = 240
Board Name: XDS510_C6748
Cpu Name: ICEPICK_C_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
运行XDS510USB_probe.bat出现问题:
Event3 pin read back of one failed.
Counter1 carry bit test failed at bit ff.
这是什么问题,要怎么解决啊?????????????