This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x LCD问题

Other Parts Discussed in Thread: AM3359

我用am335x带奇美7寸1024*600的LCD只能在驱动中跑800*480.才能点亮。用正常1024*600时提示kmalloc for frame buffer failed,还打印出很多 ------------[ cut here ]------------ [    1.338195] WARNING: at mm/page_alloc.c:2095 __alloc_pages_nodemask+0x45c/0x618() [    1.346069] Modules linked in: [    1.349273] Backtrace: [    1.351898] [<c0017978>] (dump_backtrace+0x0/0x110) from [<c04349ac>] (dump_stack+0x18/0x1c) [    1.360778]  r6:c0525c2c r5:0000082f r4:00000000 r3:c06130c8 [    1.366790] [<c0434994>] (dump_stack+0x0/0x1c) from [<c003d6a8>] (warn_slowpath_common+0x5c/0x6c) [    1.376159] [<c003d64c>] (warn_slowpath_common+0x0/0x6c) from [<c003d6dc>] (warn_slowpath_null+0x24/0x2c) [    1.386230]  r8:00000000 r7:00000000 r6:c06505b4 r5:c05f40b8 r4:c066c2a8 [    1.393096] r3:00000009 [    1.395904] [<c003d6b8>] (warn_slowpath_null+0x0/0x2c) from [<c00815e0>] (__alloc_pages_nodemask+0x45c/0x618) [    1.406341] [<c0081184>] (__alloc_pages_nodemask+0x0/0x618) from [<c0019d18>] (__dma_alloc+0xa4/0x300) [    1.416168] [<c0019c74>] (__dma_alloc+0x0/0x300) from [<c001a008>] (dma_alloc_coherent+0x60/0x68) [    1.425537] [<c0019fa8>] (dma_alloc_coherent+0x0/0x68) from [<c042ad90>] (fb_probe+0xbc4/0xbdc) [    1.434692]  r7:00002000 r6:cf9c7e08 r5:c062e5c0 r4:c0611bf4 [    1.440673] [<c042a1cc>] (fb_probe+0x0/0xbdc) from [<c022ce04>] (platform_drv_probe+0x20/0x24) [    1.449768] [<c022cde4>] (platform_drv_probe+0x0/0x24) from [<c022b81c>] (driver_probe_device+0xc0/0x2dc) [    1.459838] [<c022b75c>] (driver_probe_device+0x0/0x2dc) from [<c022bb14>] (__device_attach+0x44/0x48) [    1.469635]  r8:00000000 r7:c06128b0 r6:00000000 r5:cf9c7e08 r4:c062e504 [    1.476745] [<c022bad0>] (__device_attach+0x0/0x48) from [<c022a480>] (bus_for_each_drv+0x64/0x90) [    1.486175]  r5:c022bad0 r4:cf9c7e08 [    1.489959] [<c022a41c>] (bus_for_each_drv+0x0/0x90) from [<c022b640>] (device_attach+0xa0/0xc0) [    1.499206]  r6:cf9c7e10 r5:cf9c7e3c r4:cf9c7e08 [    1.504089] [<c022b5a0>] (device_attach+0x0/0xc0) from [<c022adf0>] (bus_probe_device+0x2c/0x48) [    1.513336]  r6:cf9c7e10 r5:cf9c7f28 r4:cf9c7e08 r3:00000001 [    1.519317] [<c022adc4>] (bus_probe_device+0x0/0x48) from [<c02290dc>] (device_add+0x4b8/0x588) [    1.528503] [<c0228c24>] (device_add+0x0/0x588) from [<c022d4e8>] (platform_device_add+0x124/0x204) [    1.538055] [<c022d3c4>] (platform_device_add+0x0/0x204) from [<c0034b38>] (omap_device_register+0x3c/0x5c) [    1.548309]  r7:c051620c r6:00000000 r5:cf9c8d40 r4:cf9c7e00 [    1.554321] [<c0034afc>] (omap_device_register+0x0/0x5c) from [<c0034c60>] (omap_device_build_ss+0x108/0x14c) [    1.564758]  r4:cf9c7e00 r3:00000000 [    1.568511] [<c0034b58>] (omap_device_build_ss+0x0/0x14c) from [<c0034cf8>] (omap_device_build+0x54/0x5c) [    1.578613] [<c0034ca4>] (omap_device_build+0x0/0x5c) from [<c05bb62c>] (am33xx_register_lcdc+0x70/0xb4) [    1.588623] [<c05bb5bc>] (am33xx_register_lcdc+0x0/0xb4) from [<c0031b18>] (lcdc_init+0x98/0xb8) [    1.597869]  r6:00000000 r5:00000002 r4:c0605a2c [    1.602752] [<c0031a80>] (lcdc_init+0x0/0xb8) from [<c00319c4>] (am335x_evm_setup+0x120/0x1a0) [    1.611816]  r6:cf8a9220 r5:c065948c r4:c061168c r3:c0031a80 [    1.617828] [<c00318a4>] (am335x_evm_setup+0x0/0x1a0) from [<c023d080>] (at24_probe+0x50c/0x57c) [    1.627075]  r5:cf9c5f40 r4:cf8a9200 [    1.630859] [<c023cb74>] (at24_probe+0x0/0x57c) from [<c02df310>] (i2c_device_probe+0xa8/0xec) [    1.639923] [<c02df268>] (i2c_device_probe+0x0/0xec) from [<c022b81c>] (driver_probe_device+0xc0/0x2dc) [    1.649810]  r6:c0653330 r5:c067aab0 r4:cf8a9220 r3:c02df268 [    1.655822] [<c022b75c>] (driver_probe_device+0x0/0x2dc) from [<c022bacc>] (__driver_attach+0x94/0x98) [    1.665618]  r8:00000000 r7:00000000 r6:cf8a9254 r5:c06331bc r4:cf8a9220 [    1.672698] [<c022ba38>] (__driver_attach+0x0/0x98) from [<c022a780>] (bus_for_each_dev+0x58/0x84) [    1.682128]  r6:00000000 r5:c022ba38 r4:c06331bc r3:c022ba38 [    1.688110] [<c022a728>] (bus_for_each_dev+0x0/0x84) from [<c022b414>] (driver_attach+0x24/0x28) [    1.697387]  r6:cf9931c0 r5:c063ed1c r4:c06331bc [    1.702239] [<c022b3f0>] (driver_attach+0x0/0x28) from [<c022b080>] (bus_add_driver+0x19c/0x26c) [    1.711517] [<c022aee4>] (bus_add_driver+0x0/0x26c) from [<c022c070>] (driver_register+0x80/0x138) [    1.720947] [<c022bff0>] (driver_register+0x0/0x138) from [<c02df764>] (i2c_register_driver+0x38/0xe8) [    1.730773]  r8:00000000 r7:00000000 r6:cf81c000 r5:c05f12fc r4:c0633194 [    1.737670] r3:c063ed1c [    1.740417] [<c02df72c>] (i2c_register_driver+0x0/0xe8) from [<c05d3da8>] (at24_init+0x50/0x54) [    1.749603]  r5:c05f12fc r4:c0658700 [    1.753356] [<c05d3d58>] (at24_init+0x0/0x54) from [<c000876c>] (do_one_initcall+0x3c/0x180) [    1.762268] [<c0008730>] (do_one_initcall+0x0/0x180) from [<c05b3884>] (kernel_init+0x9c/0x130) [    1.771453] [<c05b37e8>] (kernel_init+0x0/0x130) from [<c0040728>] (do_exit+0x0/0x67c) [    1.779785]  r5:c05b37e8 r4:00000000 [    1.783599] ---[ end trace c696f12f152aa029 ]--- [    1.788482]

da8xx_lcdc da8xx_lcdc.0: GLCD: kmalloc for frame buffer failed  。请问我要怎么修改LCD驱动?错误在fb_probe()函数。但不知道怎么改。

  • 似乎需要配置成16bit的才可以,你是不是配成24bit了

  • Yaoming Qin 你好。我现在要用1024*600的屏。用的是32的BPP。请问要怎修改。谢谢用的是最新的05.05的EVM开发环境。用16位的显示只能显示屏的上半部分,还是两个桌面一起显示的。就是ti的ui起来后是两个一模一样的桌面。出现错误的地方在DMA_ALLOC....()函数里。但是跟了好久的代码硬是没看明白怎么改。是不是335x里面规定了framebuffer的大小?如是,在哪改?

  • 你看看 board-am335xevm.c 里面的 结构体

    static struct lcd_ctrl_config lcd_cfg = {

    &disp_panel,

    .ac_bias = 255,

    .ac_bias_intrpt = 0,

    .dma_burst_sz = 16,

    .bpp = 32,

    .fdd = 0x80,

    .tft_alt_mode = 0,

    .stn_565_mode = 0,

    .mono_8bit_mode = 0,

    .invert_line_clock = 1,

    .invert_frm_clock = 1,

    .sync_edge = 0,

    .sync_ctrl = 1,

    .raster_order = 0,

    };

  • Yaoming Qin 不好意思,我不知道你是没理解我还是我没理解你的意思。如果你指在这个结构体里把BPP改为16,那就不必试了。这个结构体我改了试过的。我的屏是32的BPP用16或24的都不能正常显示,颜色偏差还厉害。我现在是要用32位1024*600的屏能正常显示,就是在dma_alloc_coherent()函数里PAGE为0,开辟空间不成功。现在还在跟代码中,不知道是不是TI驱动定死了内存分配越界了才不成功还是其他原因。求指导

  • 你好,你的问题解决了吗,我遇到同样的问题,
    AM3359 24bit 1024*768 LCD  出错“LCD: kmalloc for frame buffer failed”?
     [    1.308959]  da8xx_lcdc.0: alias fck already exists
     [    1.314666] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
     [    1.323120] ------------[ cut here ]------------ [    1.328033] WARNING: at mm/page_alloc.c:2110 __alloc_pages_nodemask+0x458/0x62c()
     [    1.335906] Modules linked in:
     [    1.339141] Backtrace:
     [    1.341735] [<c001803c>] (dump_backtrace+0x0/0x10c) from [<c04d5438>] (dump_stack+0x18/0x1c)
     [    1.350646]  r7:00000009 r6:0000083e r5:c00840a0 r4:00000000
     [    1.356628] [<c04d5420>] (dump_stack+0x0/0x1c) from [<c003d284>] (warn_slowpath_common+0x54/0x6c)
     [    1.365997] [<c003d230>] (warn_slowpath_common+0x0/0x6c) from [<c003d2c0>] (warn_slowpath_null+0x24/0x2c)
     [    1.376068]  r9:c06f3ce0 r8:00000000 r7:00000000 r6:c069e110 r5:c0708028
     [    1.382965] r4:00000000 [    1.385742] [<c003d29c>] (warn_slowpath_null+0x0/0x2c) from [<c00840a0>] (__alloc_pages_nodemask+0x458/0x62c)
     [    1.396209] [<c0083c48>] (__alloc_pages_nodemask+0x0/0x62c) from [<c001a2c8>] (__dma_alloc+0x90/0x308)
     [    1.406036] [<c001a238>] (__dma_alloc+0x0/0x308) from [<c001a5d0>] (dma_alloc_coherent+0x5c/0x68)
     [    1.415374] [<c001a574>] (dma_alloc_coherent+0x0/0x68) from [<c04cd0cc>] (fb_probe+0x7a8/0xbc4)
     [    1.424530]  r7:cf9bc608 r6:007d0000 r5:cf9c1a54 r4:c06d2844
     [    1.430541] [<c04cc924>] (fb_probe+0x0/0xbc4) from [<c02648e4>] (platform_drv_probe+0x20/0x24)
     [    1.439605] [<c02648c4>] (platform_drv_probe+0x0/0x24) from [<c026342c>] (driver_probe_device+0xa0/0x1b0)
     [    1.449707] [<c026338c>] (driver_probe_device+0x0/0x1b0) from [<c0263618>] (__device_attach+0x44/0x48)
     [    1.459503]  r9:c002ff2c r8:c0714d8c r7:00000000 r6:c02635d4 r5:cf9bc608
     [    1.466400] r4:c06d2788
     [    1.469177] [<c02635d4>] (__device_attach+0x0/0x48) from [<c02628d8>] (bus_for_each_drv+0x68/0x94)
     [    1.478607]  r5:cf81dc48 r4:cf9bc608
     [    1.482391] [<c0262870>] (bus_for_each_drv+0x0/0x94) from [<c02636e4>] (device_attach+0x9c/0xc0)
     [    1.491638]  r7:c06be7f0 r6:00000000 r5:cf9bc63c r4:cf9bc608
     [    1.497650] [<c0263648>] (device_attach+0x0/0xc0) from [<c02626dc>] (bus_probe_device+0x2c/0x48)
     [    1.506896]  r7:c06be7f0 r6:00000000 r5:cf9bc610 r4:cf9bc608
     [    1.512878] [<c02626b0>] (bus_probe_device+0x0/0x48) from [<c0261554>] (device_add+0x4c4/0x590)
     [    1.522064] [<c0261090>] (device_add+0x0/0x590) from [<c0264f80>] (platform_device_add+0x100/0x19c)
     [    1.531616] [<c0264e80>] (platform_device_add+0x0/0x19c) from [<c00332dc>] (omap_device_register+0x28/0x2c)
     [    1.541870]  r7:c05c6868 r6:00000000 r5:cf9c4e00 r4:cf9bc600
     [    1.547851] [<c00332b4>] (omap_device_register+0x0/0x2c) from [<c00338b4>] (omap_device_build_ss+0x108/0x144)
     [    1.558319] [<c00337ac>] (omap_device_build_ss+0x0/0x144) from [<c0033944>] (omap_device_build+0x54/0x5c)
     [    1.568420] [<c00338f0>] (omap_device_build+0x0/0x5c) from [<c06685a0>] (am33xx_register_lcdc+0x64/0xb0)
     [    1.578399]  r4:00000000 [    1.581085] [<c066853c>] (am33xx_register_lcdc+0x0/0xb0) from [<c002f778>] (lcdc_init+0x30/0x60)
     [    1.590332]  r6:00000001 r5:00000001 r4:c06bd128
     [    1.595245] [<c002f748>] (lcdc_init+0x0/0x60) from [<c002f1f8>] (_configure_device+0x70/0xdc)
     [    1.604217] [<c002f188>] (_configure_device+0x0/0xdc) from [<c0030130>] (am335x_evm_setup+0x204/0x4ac)
     [    1.614044]  r7:00000000 r6:cf8a0820 r5:00000000 r4:c06bdac0
     [    1.620025] [<c002ff2c>] (am335x_evm_setup+0x0/0x4ac) from [<c0276794>] (at24_probe+0x45c/0x4e4)
     [    1.629272]  r6:cf8a0820 r5:cf8a0800 r4:cf9c3d40
     [    1.634185] [<c0276338>] (at24_probe+0x0/0x4e4) from [<c032c66c>] (i2c_device_probe+0xb4/0xec)
     [    1.643249] [<c032c5b8>] (i2c_device_probe+0x0/0xec) from [<c026342c>] (driver_probe_device+0xa0/0x1b0)
     [    1.653137]  r7:c06d7558 r6:cf8a0854 r5:c0714db0 r4:cf8a0820 [    1.659118] [<c026338c>] (driver_probe_device+0x0/0x1b0) from [<c02635d0>] (__driver_attach+0x94/0x98)
     [    1.668945]  r9:00000000 r8:00000000 r7:00000000 r6:cf8a0854 r5:c06d7558
     [    1.675842] r4:cf8a0820 [    1.678588] [<c026353c>] (__driver_attach+0x0/0x98) from [<c0262be0>] (bus_for_each_dev+0x68/0x94)
     [    1.688049]  r7:00000000 r6:c026353c r5:cf81dec8 r4:c06d7558
     [    1.694030] [<c0262b78>] (bus_for_each_dev+0x0/0x94) from [<c026327c>] (driver_attach+0x24/0x28)
     [    1.703277]  r7:00000000 r6:cf9c3ec0 r5:c06e3db0 r4:c06d7558
     [    1.709259] [<c0263258>] (driver_attach+0x0/0x28) from [<c0262448>] (bus_add_driver+0xa8/0x23c)
     [    1.718444] [<c02623a0>] (bus_add_driver+0x0/0x23c) from [<c0263c34>] (driver_register+0x80/0x144)
     [    1.727905] [<c0263bb4>] (driver_register+0x0/0x144) from [<c032cab0>] (i2c_register_driver+0x34/0xbc)
     [    1.737701]  r9:00000000 r8:00000000 r7:00000013 r6:00000000 r5:c06f4180
     [    1.744598] r4:c06d7530
     [    1.747375] [<c032ca7c>] (i2c_register_driver+0x0/0xbc) from [<c067b8f8>] (at24_init+0x48/0x54)
     [    1.756530]  r5:c06f4180 r4:c069ab4c
     [    1.760314] [<c067b8b0>] (at24_init+0x0/0x54) from [<c0008610>] (do_one_initcall+0x44/0x1a4)
     [    1.769195] [<c00085cc>] (do_one_initcall+0x0/0x1a4) from [<c0660288>] (kernel_init+0x80/0x124)
     [    1.778381] [<c0660208>] (kernel_init+0x0/0x124) from [<c0040884>] (do_exit+0x0/0x6ac)
     [    1.786712]  r5:c0660208 r4:00000000
     [    1.790557] ---[ end trace b4622b5c66012fd7 ]---
     [    1.795440] da8xx_lcdc da8xx_lcdc.0: GLCD: kmalloc for frame buffer failed
     [    1.802703] da8xx_lcdc: probe of da8xx_lcdc.0 failed with error -22

    AM3359 LCD 16bit RGB   24Bit 现已经换成BGR。
    我的修改如下:board-am335xevm.c
    static const struct display_panel disp_panel = {
        WVGA,
        16,
        24,
        COLOR_ACTIVE,
    };
    static struct lcd_ctrl_config lcd_cfg = {
        &disp_panel,
        .ac_bias        = 255,
        .ac_bias_intrpt        = 0,
        .dma_burst_sz        = 16,
        .bpp            = 24,
        .fdd            = 0x80,
        .tft_alt_mode        = 0,
        .stn_565_mode        = 0,
        .mono_8bit_mode        = 0,
        .invert_line_clock    = 1,
        .invert_frm_clock    = 1,
        .sync_edge        = 0,
        .sync_ctrl        = 1,
        .raster_order        = 0,
    };
    在am335x_evm_defconfig文件:FB_DA8XX_CONSISTENT_DMA_SIZE 已改为14,还是出现如上错误。

    知道是什么原因吗?求指导。。

  • 你好,你按下面 改下,下面是原因和步骤。 推荐你以后还是去ti的e2e网站问问题吧,这里没什么人回答。

    It is Linux kernel limit. AM335x Linux kernel has 1024 number pages, than the page size is 4096 bytes.

    So "dma_alloc_coherent()" can't allocating more than 4MB.

    Fellow these step, resolve this problem:

    1. Please, modify the "#define MAX_ORDER 12" in the include/linux/mmzone.h

    2. Please tune menuconfig option, FB_DA8XX_CONSISTENT_DMA_SIZE [=5] or more

    3. Rebuild your Linux kernel

    BR

  • 你好,我用am3359带奇美10‘4的屏,1024*768*24,按照你提供的步骤,还是出现”GLCD: kmalloc for frame buffer failed“错误,

    MAX_ORDER 12

    FB_DA8XX_CONSISTENT_DMA_SIZE [=6]

    感觉FB_DA8XX_CONSISTENT_DMA_SIZE的值没有被修改。。。。

    请问还有其它需要注意的地方吗?

    我给TI已经发了邮件现在还没有回。。。

  • 我用的是1024*600*32位的。改了那些之后就malloc成功了。你把定义MAX_ORDER 12的那个判断注释掉,自己定义下#define MAX_ORDER 12。其他的好像没有什么了 ,可以把DMA_SIZE扩大在试试。

  • 非常感谢,,,,,将原定义MAX_ORDER 12的那个判断注释掉,自己定义#define MAX_ORDER 12 ,后成功了,,,谢谢你的指点。

  • 别客气,能帮上忙我也很高兴。互相学习。