This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于AM5718通过SD卡烧写EMMC问题

Other Parts Discussed in Thread: TMDXIDK5718, AM5718

新购买了一套TMDXIDK5718,官网上下载了SDK,文件是ti-processor-sdk-android-am57xx-evm-04.02.00.09-Linux-x86-Install.bin, 然后通过statted guide(processors.wiki.ti.com/.../Processor_SDK_Android_Getting_Started_Guide)操作,一直未能成功。请各位帮忙看看是什么原因,谢谢!

第5步Run the Setup Script,串口信息如下:

zhubinbin@zhubinbin-VirtualBox:~/ti-processor-sdk-android-am57xx-evm-04.02.00.09$ sudo ./setup.sh 

Just a simple wrapper over the fastboot.sh to set the appropriate paths.

--------------------------------------------------------------------------------"

This step will set up minicom (serial communication application) for

SDK development

For boards that contain a USB-to-Serial converter on the board such as:

* BeagleBone

* Beaglebone Black

* AM335x EVM-SK

* AM57xx EVM

* K2H, K2L, and K2E EVMs

the port used for minicom will be automatically detected. By default Ubuntu

will not recognize this device. Setup will add a udev rule to

/etc/udev/ so that from now on it will be recognized as soon as the board is

plugged in.

For other boards, the serial will defualt to /dev/ttyS0. Please update based

on your setup.

--------------------------------------------------------------------------------

NOTE: If your using any of the above boards simply hit enter

and the correct port will be determined automatically at a

later step.  For all other boards select the serial port

that the board is connected to.

Which serial port do you want to use with minicom?

[ /dev/ttyUSB0 ] 

Copied existing /home/zhubinbin/.minirc.dfl to /home/zhubinbin/.minirc.dfl.old

Configuration saved to /home/zhubinbin/.minirc.dfl. You can change it further from inside

minicom, see the Software Development Guide for more information.

--------------------------------------------------------------------------------

--------------------------------------------------------------------------------

This step will set up the u-boot variables for booting the EVM.

--------------------------------------------------------------------------------

--------------------------------------------------------------------------------

Would you like to create a minicom script to configure the board (y/n)?

[ y ] y

Successfully wrote /home/zhubinbin/ti-processor-sdk-android-am57xx-evm-04.02.00.09/bin/setupBoard.minicom

Detecting connection to board... /dev/ttyUSB2

--------------------------------------------------------------------------------

Would you like to run the setup script now (y/n)?

Please connect the USB and USB/serial cables as described in the Quick Start

Guide. Once answering 'y' on the prompt below, you will have 300 seconds to

connect the board and power cycle it before the setup times out.

After successfully executing this script, your EVM will be set up. After power

cycling the board, you will be able to connect to it by executing 'minicom -w'

or by using the 'adb' utility. If you prefer a windows host, you can set up

Tera Term as explained in the Software Developer's Guide.

[ y ] y

Welcome to minicom 2.7

OPTIONS: I18n 

Compiled on Jan  1 2014, 17:13:19.

Port /dev/ttyUSB2, 10:10:56

Press CTRL-A Z for help on special keys

U-Boot SPL 2016.05-g6f6aaabf5a (Dec 23 2017 - 13:14:49)

DRA722-GP ES2.0

Trying to boot from MMC1

no pinctrl for hs200_1_8v

no pinctrl for ddr_1_8v

no pinctrl for hs200_1_8v

reading args

spl_load_image_fat_os: error reading image args, err - -1

reading u-boot.img

reading u-boot.img

reading u-boot.img

reading u-boot.img

                                                                                

U-Boot 2016.05-g6f6aaabf5a (Dec 23 2017 - 13:14:49 -0500)                       

                                                                                

CPU  : DRA722-GP ES2.0                                                          

Model: TI AM5718 IDK                                                            

Board: AM571x IDK REV 1.3B                                                      

DRAM:  1 GiB                                                                    

MMC:   mmc@4809c000: fail to find sdr104 mode FDT_ERR_NOTFOUND                  

no pinctrl for sdr104                                                           

mmc@4809c000: fail to find ddr50 mode FDT_ERR_NOTFOUND                          

no pinctrl for ddr50                                                            

mmc@4809c000: fail to find sdr50 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr50                                                            

mmc@4809c000: fail to find sdr25 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr25                                                            

mmc@4809c000: fail to find sdr12 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr12                                                            

OMAP SD/MMC: 0, OMAP SD/MMC: 1                                                  

** First descriptor is NOT a primary desc on 1:1 **                             

GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645       

part_get_info_efi: *** ERROR: Invalid GPT ***                                   

GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645       

part_get_info_efi: *** ERROR: Invalid Backup GPT ***                            

ERROR: cannot find partition: 'userdata'                                        

                                                                                

at /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/am57xx_evm-li

nux-gnueabi/u-boot-ti-android/2016.05+gitAUTOINC+6f6aaabf5a-r0/git/arch/arm/cpu/

armv7/omap-common/utils.c:199/mmc_get_part_size()                               

Warning: fastboot.userdata_size: unable to calc                                 

SCSI:  SATA link 0 timeout.                                                     

AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode                       

flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst                

scanning bus for devices...                                                     

Found 0 device(s).                                                              

Net:   eth0: ethernet@48484000                                                  

Hit any key to stop autobo 0                                                    

=>env default -f -a                                                             

## Resetting to default environment                                             

=>setenv partitions ${partitions_android}                                       

=>setenv bootpart 0:1                                                           

=>setenv rootpart 0:2                                                           

=>setenv bootdir                                                                

=>setenv devtype mmc                                                            

=>setenv finduuid 'part uuid ${devtype} ${rootpart} uuid'                       

=>setenv optargs ${bootargs}                                                    

=>setenv dofastboot 1                                                           

=>saveenv                                                                       

Saving Environment to MMC...                                                    

Writing to MMC(1)... done                                                       

=>reset                                                                         

resetting ...                                                                   

                                                                                

U-Boot SPL 2016.05-g6f6aaabf5a (Dec 23 2017 - 13:14:49)                         

DRA722-GP ES2.0                                                                 

Trying to boot from MMC1                                                        

no pinctrl for hs200_1_8v                                                       

no pinctrl for ddr_1_8v                                                         

no pinctrl for hs200_1_8v                                                       

reading args                                                                    

spl_load_image_fat_os: error reading image args, err - -1                       

reading u-boot.img                                                              

reading u-boot.img                                                              

reading u-boot.img                                                              

reading u-boot.img                                                              

                                                                                

                                                                                

U-Boot 2016.05-g6f6aaabf5a (Dec 23 2017 - 13:14:49 -0500)                       

                                                                                

CPU  : DRA722-GP ES2.0                                                          

Model: TI AM5718 IDK                                                            

Board: AM571x IDK REV 1.3B                                                      

DRAM:  1 GiB                                                                    

MMC:   mmc@4809c000: fail to find sdr104 mode FDT_ERR_NOTFOUND                  

no pinctrl for sdr104                                                           

mmc@4809c000: fail to find ddr50 mode FDT_ERR_NOTFOUND                          

no pinctrl for ddr50                                                            

mmc@4809c000: fail to find sdr50 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr50                                                            

mmc@4809c000: fail to find sdr25 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr25                                                            

mmc@4809c000: fail to find sdr12 mode FDT_ERR_NOTFOUND                          

no pinctrl for sdr12                                                            

OMAP SD/MMC: 0, OMAP SD/MMC: 1                                                  

** First descriptor is NOT a primary desc on 1:1 **                             

GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645       

part_get_info_efi: *** ERROR: Invalid GPT ***                                   

GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645       

part_get_info_efi: *** ERROR: Invalid Backup GPT ***                            

ERROR: cannot find partition: 'userdata'                                        

                                                                                

at /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/am57xx_evm-li

nux-gnueabi/u-boot-ti-android/2016.05+gitAUTOINC+6f6aaabf5a-r0/git/arch/arm/cpu/

armv7/omap-common/utils.c:199/mmc_get_part_size()                               

Warning: fastboot.userdata_size: unable to calc                                 

SCSI:  SATA link 0 timeout.                                                     

AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode                       

flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst                

scanning bus for devices...                                                     

Found 0 device(s).                                                              

Net:                                                                            

Warning: ethernet@48484000 using MAC address from ROM                           

eth0: ethernet@48484000                                                         

Hit any key to stop autoboot:  0                                                

Boot fastboot requested, resetting dofastboot ...                               

Saving Environment to MMC...                                                    

Writing to redundant MMC(1)... done                                             

Booting into fastboot ...

/home/zhubinbin/ti-processor-sdk-android-am57xx-evm-04.02.00.09

You can manually run minicom in the future with this setup script using:

 $ minicom -S /home/zhubinbin/ti-processor-sdk-android-am57xx-evm-04.02.00.09/bin/setupBoard.minicom

--------------------------------------------------------------------------------

Fastboot: ./fastboot

Image location: /home/zhubinbin/ti-processor-sdk-android-am57xx-evm-04.02.00.09/board-support/prebuilt-images/

No device detected. Please ensure that fastboot is running on the target device

ti-processor-sdk-android-am57xx-evm-04.02.00.09-Linux-x86-Install.bin