This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

达芬奇 DM368 DVSDK4.02平台 采集500W (2432X2048)One-shot模式采集,图像宽度只支持2176个像素,所以图像宽度超出的部分2432-2176,这些像素宽度图像无法正常显示,请问达芬奇 DM368专家解答一下如何才能正常采集500W 2432X2048分辨率正常显示的问题,谢谢!



各位专家你们好:

现用DM368 dvsdk4.02平台采集500W 2432X2048分辨率的视频流,前端用FPGA采集RAW数据然后转换为YUV420SP格式做H264编码,但是由于YUV420SP最大支持的图像宽度只有2176个像素,我们采集的图像分辨率是2432X2048所以,图像宽度超出的部分会变化,无法显示,请看附件 TI DVSDK 4.0.2 2464X2048.zip里的图片TI DVSDK 4.0.2 2464X2048.jpg,请问各位专家 DM368 如何才能在DVSDK4.02平台上采集500 W 2432X2048这么大分辨率的图像呢?谢谢!

TI DVSDK 4.0.2 2464X2048.zip
  • DM36x IPNC已经实现这部分功能.主要原理是图像分成左右两部分过resizer.

  • Feng Dong 大哥,您好,您用过DM368 TI DVSDK 4.0 采集500W 2432X2048分辨率吗?因为TI DVSDK 4.0里的preview 和resizer 跟APPRO 2.6 处理2592X1920 500W的架构不通,我用TI DVSDK 4.02 里的psp下的do_preview_resizer.c,测试,图像不正常,希望指点一下,谢谢!

  • 两边的架构是不同.没有在dvsdk上搞过5M.还是建议用ipnc的框架.否则就直接在应用层将其分成两部分,分别过resizer.

  • DEAR Feng Dong ,现在我在TI DVSDK 4.0 DM368平台上已经解决了500W 采集的问题,现在再问您一个问题,如何提高DM368 前端采集帧率,现在FPGA前端送过来的帧率是8FPS,但是,实际采集到的只有6-7帧,请问 Fend Dong如何提高前端采集帧率帧率,我的是500W 的。谢谢!

  • 楼主请问ISIF进来几帧?通过IPIPE后每秒几帧?

  • 现在想请教您一个问题:现在用DM368 APPRO 4.0的平台采集500W 2432X2048分辨率的图像,发现实际采集的帧率比前段FPGA送来的帧率少1-2帧,前段FPGA送过来的帧率是8.5帧率,但是,DM368 采集的平均帧率才7.5帧率,有可能还会少点,大概6帧率多,想请问您如何提高采集编码帧率,实际采集的跟去前段FPGA送来的帧率相同,谢谢!

    我抓DM368 APPRO 4.0 打印的LOG如下:

    Module   | Avg Time/Frame | Frame-rate | Total time | Total Frames |

    CAPTURE  |         134.96 |       7.41 |      40624 |          301 |

    IPIPE          |          33.94 |      29.47 |      20431 |          602 |

    ENCODE0  |          77.10 |      12.97 |      23208 |          301 |

    STREAM    |            2.40 |     417.48 |          721 |            301  |

  • 我测的9p031的ipnc大概到9-10帧,主要要查的是前端,isif以及ipipe的时钟配置

  • 那请问 Feng Dong 大哥,我500W 2432X2048 分辨率采集FPAG送过来的图像,我需要配置IPIPE时钟分频吗?如果需要如何配置?前端采集capture部分需要对什么时钟做特殊配置吗?如果需要又需要做哪些时钟配置?谢谢!前端FPGA像素时钟是给的50-60MB赫兹,采集一次需要的时间大概是135MS左右,希望FENG DONG 大哥指导一下,谢谢了!

  • 那请问 Feng Dong 大哥,我500W 2432X2048 分辨率采集FPAG送过来的图像,我需要配置IPIPE时钟分频吗?如果需要如何配置?前端采集capture部分需要对什么时钟做特殊配置吗?如果需要又需要做哪些时钟配置?谢谢!前端FPGA像素时钟是给的50-60MB赫兹,采集一次需要的时间大概是135MS左右,希望FENG DONG 大哥指导一下,谢谢了!

  • 对于5M由于要走两次,第一次通过isif导入memory,第二次才是通过ipipe转成yuv,所以你要查vpfe中ipipe的clock的设置.

    建议还是使用ipnc吧.

  • 请问 FENG DONG 大哥,如何调高ipipe 和ISIF的时钟,谢谢!