This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

QDMA中触发字的理解?



在QDMA中,触发字的设置如右图:         

在QCHMAPn中设置了通道和param的联系,同时设置了触发字:例如写寄存器QCHMAP0和PaRAM 0相连,同时设置触发字为7。在link触发传输时,要将触发字写在最后一个被link的PaRAM的CCNT的位置上写1,才能触发传输?这是为什么,难道不是设置的触发字是什么,在写触发字的时候就写几吗?

1:在QCHMAP中设置的触发字和最后为了触发通道所写的触发字的关系是什么?

2:从示意图上看,触发字是一定要写在PaRAM的CCNT位置上的,该PaRAM必须是在QCHMAP 中设置的PAENTRY,这样的理解对吗?

3:每一个触发字唯一地标示了一个QDMA通道和与该通道相联系的PaRAM,这样理解触发字对吗?

看了文档的相关内容,但是对内容的理解比较模糊,还望解答,谢谢!!