This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于KeyStone_SRIO例子中DDR的初始化



TI guys:

我在使用KeyStone_SRIO的例子在6670和6678的EVM板上进行自环测试,Digital Loopback都能够通过~但我观察到两块EVM板用的都是同一款三星DDR,每块DSP也都配备了4块这样的DDR,但Nyquist_EVM_DDR_Init和Shannon_EVM_DDR_Init这两个函数却差别非常大,引用如下:

6678中row size配置的是13bit

(DDR_ROW_SIZE_13_BIT<<CSL_EMIF4F_SDRAM_CONFIG_REG_ROWSIZE_SHIFT)

6670中row size 配置的是14bit

DR_ROW_SIZE_14_BIT<<CSL_EMIF4F_SDRAM_CONFIG_REG_ROWSIZE_SHIFT)

另外,6670中有关初始化leveling的代码与6678中有截然不同的配置

6670:

//initial vale for leveling
/*WRLVL_INIT_RATIO*/
boot_cfg_regs->DDR3_CONFIG_REG[2] = 0x0F;
boot_cfg_regs->DDR3_CONFIG_REG[3] = 0x0F;
boot_cfg_regs->DDR3_CONFIG_REG[4] = 0x20;
boot_cfg_regs->DDR3_CONFIG_REG[5] = 0x24;
boot_cfg_regs->DDR3_CONFIG_REG[6] = 0x33;
boot_cfg_regs->DDR3_CONFIG_REG[7] = 0x38;
boot_cfg_regs->DDR3_CONFIG_REG[8] = 0x21;
boot_cfg_regs->DDR3_CONFIG_REG[9] = 0x29;
boot_cfg_regs->DDR3_CONFIG_REG[10] = 0x0 ;

/*GTLVL_INIT_RATIO*/
boot_cfg_regs->DDR3_CONFIG_REG[14] = 0x7B;
boot_cfg_regs->DDR3_CONFIG_REG[15] = 0x7B;
boot_cfg_regs->DDR3_CONFIG_REG[16] = 0x8D;
boot_cfg_regs->DDR3_CONFIG_REG[17] = 0x89;
boot_cfg_regs->DDR3_CONFIG_REG[18] = 0xC0;
boot_cfg_regs->DDR3_CONFIG_REG[19] = 0xBC;
boot_cfg_regs->DDR3_CONFIG_REG[20] = 0xC3;
boot_cfg_regs->DDR3_CONFIG_REG[21] = 0xBB;
boot_cfg_regs->DDR3_CONFIG_REG[22] = 0x0 ;

6678:

//initial vale for leveling
/*GTLVL_INIT_RATIO*/
boot_cfg_regs->DDR3_CONFIG_REG[14] = 0xA1;
boot_cfg_regs->DDR3_CONFIG_REG[15] = 0x9E;
boot_cfg_regs->DDR3_CONFIG_REG[16] = 0xA7;
boot_cfg_regs->DDR3_CONFIG_REG[17] = 0xA9;
boot_cfg_regs->DDR3_CONFIG_REG[18] = 0xCA;
boot_cfg_regs->DDR3_CONFIG_REG[19] = 0xBE;
boot_cfg_regs->DDR3_CONFIG_REG[20] = 0xDD;
boot_cfg_regs->DDR3_CONFIG_REG[21] = 0xDD;
boot_cfg_regs->DDR3_CONFIG_REG[22] = 0xBA;

/*WRLVL_INIT_RATIO*/
boot_cfg_regs->DDR3_CONFIG_REG[2] = 0x20;
boot_cfg_regs->DDR3_CONFIG_REG[3] = 0x24;
boot_cfg_regs->DDR3_CONFIG_REG[4] = 0x3A;
boot_cfg_regs->DDR3_CONFIG_REG[5] = 0x38;
boot_cfg_regs->DDR3_CONFIG_REG[6] = 0x51;
boot_cfg_regs->DDR3_CONFIG_REG[7] = 0x5E;
boot_cfg_regs->DDR3_CONFIG_REG[8] = 0x5E;
boot_cfg_regs->DDR3_CONFIG_REG[9] = 0x5E;
boot_cfg_regs->DDR3_CONFIG_REG[10] = 0x44;

以及6670中多一段这样的代码:

/*the PHY_RESET is pulsed (0 -> 1 -> 0) to latch these
leveling configuration values into the PHY logic.*/
DDR_Regs->DDR_PHY_CTRL_1 &= ~(0x00008000);
DDR_Regs->DDR_PHY_CTRL_1 |= (0x00008000);
DDR_Regs->DDR_PHY_CTRL_1 &= ~(0x00008000);

6678同样有leveling,为什么没这样的配置?

之所以有这么多的问题,是因为当我把KeyStone_SRIO放在一块有双6670DSP,每块DSP只有两块同样型号三星DDR的板上跑单核digital loopback,DDR初始化不成功,DDR_Regs->STATUS这一部的三个状态全部为1,timeout~想请教一下为什么两块EVM板DDR初始化函数有这么大的区别,以及如果变成了2块DDR对应一块DSP,在一只时钟频率的基础上应该如何修改DDR初始化代码?谢谢