This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L2RAM和L2cache配置的问题



目前正在使用C6713,在用CCS6.1新建工程时,软件自动生成的CMD文件中,是这么写的:  

IRAM     o = 0x00000000  l = 0x00030000  /* 192kB - Internal RAM */
L2RAM    o = 0x00030000  l = 0x00010000  /* 64kB - Internal RAM/CACHE */

但是我在文档中看到复位后默认是L2 cache disabled,就是所有全部分配到SRAM。我的问题是:

1. 如果我想把上面的L2RAM像IRAM一样直接使用,是配置成cache还是SRAM?

2. 如果我想把上面的L2RAM像IRAM一样直接使用,是不是直接写IRAM     o = 0x00000000  l = 0x00040000 就可以?

3. L2RAM在上电且不配置相应寄存器时全部设为SRAM,那为什么还要单独列出来?