This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 VPSS显示驱动的标清输出设置



你好,我们现在自己开发DM8168板子,DA芯片ADV7179接在8168的vout1输出口,即DVO1,需要从该接口输出标清(PAL/NTSC)信号。该口同时也是HDMI信号的输出口。

驱动开发用的软件框架是DVRRDK 2.0的,实验使用vdec+vdis这个demo。这个demo支持从DVO1输出高清格式的视频,但并未支持输出标准的BT656视频格式。

请问如果要将demo程序改为DVO1支持PAL和NTSC制式视频输出,送给ADV7179解码显示,需要怎么修改呢?谢谢

 

  • 绑定了不好处理。你看框图DVO1和HDMI是共享了pixel clk的。你为何不用DVO2来做?

    此外,ADV7179就是个数模转换到BNC上面的, 这个功能8168上面集成SDDAC了,为何不用?

  • 现在硬件板已经做了出来,如果非必要,可能也不会改了。DVO1和HDMI共享pixel clock,但不一定要同时在ADV7179和HDMI接口输出,所以现在想知道,要使DVO1支持表情输出的修改难度大不大?DVO2上接了另一个DA芯片,提供VGA接口输出。

    此外,用SDDAC的话,出来还需要外接DA芯片吗,还是可以直接输出到BNC接口?谢谢

  • 用SDDAC的话,不用再外接DA了,但是还是存在一些的外围电路的,直接接出来效果是不好的,可以参考EVM。

    要配置DVO1也不难,就是设置好相应的时钟和同步参数,可以在demo的显示部分找到代码做参考。

    总之你这个接法就是怪,绕这个弯路。。。