This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SEED-XDS560v2 连接EVMC6657问题



系统:XP SP3
环境:CCS5.2
硬件平台:EVMC6657
仿真器:SEED-XDS560v2
现象:ccxml文件配置好后点击“test Connection”,报出错误是
“The value is "-250" (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
An attempt to access the named emulator via USCIF ECOM has failed.”

其他:用这个仿真器连接自己的6455板子没问题,可以Debug。

这个是什么问题?