This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 uboot无法识别nandflash



U-Boot 2013.01.01 (May 20 2018 - 18:09:05)

I2C:   ready
DRAM:  256 MiB
WARNING: Caches not enabled
NAND:  NAND ID is 00-00
No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment

Net:   phy_id = 508145
cpsw, usb_ether
Hit any key to stop autoboot:  0
lcd reset
Booting from nand ...

通过示波器查看,信号线有变化,gpmc_ad0-gpmc_ad7没有变化,sysboot设置没有问题,sysboot[0:4]=0x17,也做了管脚服用设置