This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320C6657与FPGA通过PCIE接口通信的问题



1、DSP与FPGA通信时,是不是可以从0x21802000地址读取到FPGA端的配置数据?如果可以,需要做什么配置?

2、如果FPGA的PCIE模块没有正常工作,那DSP端能否从0x60000000读写数据?如果可以,这些数据是临时的还是在内存的什么地方?

3、TMS320c6657评估板之间进行PCIe通信的话,需要什么接插件连接?可以直接飞线吗?

4、如果DSP端选择x1模式,是否必须使用lane0?