请问有没有人遇到过这种情况,板子是dsk6455开发板,直接import的example的helloworld(include nimu code),使用DHCPC时获取不到IP地址,就修改了localIpAddress,配置了静态地址,并在NetworkOpen中TSK_create( dtask_udp_sendhello, &tskAttrs);dtask_udp_sendhello用来发送UDP数据包,但sendto失败,返回-1,ping 也失败。请问有没有人知道可能的原因,已经查好几天了,谢谢
[C64XP_0]
TCP/IP Stack 'Hello World!' Application
Using MAC Address: 00-01-22-33-44-55
EMAC should be up and running
EMAC has been started successfully
Registeration of the EMAC Successful
Link Status: 100Mb/s Full Duplex on PHY 1
Network Added: If-1:192.168.3.121
sendto failed, return num = -1